Part Number: LDC1101
Hi,
I want to detect the vibration characteristics of a 10mm-thick aluminum alloy crossbar with a measurement range of 0.5–3mm, using the LHR (High-Resolution Inductance) mode. The sampling rate is set to 10 kSPS.
Now I need to design a sensor. According to Optimizing L Measurement Resolution for the LDC161x and LDC1101.PDF, for the LDC161x, the highest effective resolution typically occurs when fSENSOR is between 400kHz and 6MHz (for fREF=40MHz). However, it does not specify the maximum useful resolution for the LDC1101. As stated in LDC1101 Data Sheet (9.1.11 Sensor Input Divider), the reference clock frequency should be greater than 4 times the sensor frequency for optimum measurement resolution: fCLKIN>4⋅fSENSOR−MAX.
Taking these factors into account, in order to optimizing L measurement resolution, within the allowable sensor frequency range (500 kHz to 10 MHz), should the maximum useful sensor frequency be designed as 4MHz when fCLKIN=16MHz?
Thanks.