Part Number: FDC2214
我想用FDC2214做一个4通道1khz采样的设计,FDC2214可以实现么?在他手册的最前面就说到一个通道运行可以达到4.08ksps的输出速率,我想知道如果我四个通道同时运行,这个输出速率能到多少?文档中我发现,一个通道的时候,除了刚开始的稳定时间以外,就是周期性的转换时间和放大器的振幅修正时间,假设输出速率是4.08KSPS 那转换时间加上振幅修正时间约为245us,因为我可以认为转换时间小于245us,那四个通道的应用,是否可以认为转换时间也是小于245us的,在40MHZ的参考时钟下,稳定时间加开关延时约5us 是否可以认为一个通道的转换周期是250us?这样可以实现每个通道1KHZ的采样设计?在手册的底15页(中文版)有一个ENOB的概念,我不理解这个ENOB是一个什么参数,这个参数要怎么设置才合理呢?这个参数和FDC2214的分辨率(28位)有没有关系呢?