Other Parts Discussed in Thread: TPS8802, MSPM0L1306,
I am currently using the MSPM0L1306 - Launchpad and the TPS8802EVM (TPS8802 Residential Photoelectric Smoke/Carbon Monoxide Alarm Evaluation Module) sensor. My goal is to configure the TPS8802EVM to read real - time smoke and carbon monoxide data via I2C using the dual - beam smoke detector example. After my preliminary testing, I clicked on the DualRaySmoke_FR2355_MSP_TPS Version 2.6.1 GUI and confirmed a normal connection. However, I did not observe the expected changes in the infrared LED, blue LED, and reflection increment as described in the application manual for the dual - beam smoke detector using the TPS8802 and MSPM0 MCU [Demo GUI - Page 10]. Please provide me with a correct hardware connection diagram for the MSPM0L1306 - Launchpad and the TPS8802EVM, which allows me to run it in conjunction with the sdk_lp_mspm0l1306_demos_dualray_smoke_detector source code. Thank you very much.
Email:48722639@qq.com