This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS8802EVM: How to Use the Dual-Beam Smoke Detector Example Test to Connect the EVM to the MSPM0L1306 LaunchPad

Part Number: TPS8802EVM
Other Parts Discussed in Thread: TPS8802, MSPM0L1306,

I am currently using the MSPM0L1306 - Launchpad and the TPS8802EVM (TPS8802 Residential Photoelectric Smoke/Carbon Monoxide Alarm Evaluation Module) sensor. My goal is to configure the TPS8802EVM to read real - time smoke and carbon monoxide data via I2C using the dual - beam smoke detector example. After my preliminary testing, I clicked on the DualRaySmoke_FR2355_MSP_TPS Version 2.6.1 GUI and confirmed a normal connection. However, I did not observe the expected changes in the infrared LED, blue LED, and reflection increment as described in the application manual for the dual - beam smoke detector using the TPS8802 and MSPM0 MCU [Demo GUI - Page 10]. Please provide me with a correct hardware connection diagram for the MSPM0L1306 - Launchpad and the TPS8802EVM, which allows me to run it in conjunction with the sdk_lp_mspm0l1306_demos_dualray_smoke_detector source code. Thank you very much.
  Email:48722639@qq.com

  • 我目前正在使用 MSPM0L1306 -Launchpad 和 TPS8802EVM(TPS8802 住宅光电烟雾/一氧化碳报警评估模块)传感器。我的目标是使用双射线烟雾探测器示例将TPS8802EVM配置为通过 I2C 读取实时烟雾和一氧化碳数据,经过我初步测试,. 点击 DualRaySmoke_FR2355_MSP_TPS Version 2.6.1 GUI,已确认正常连接,但是、我没有观察到 使用 TPS8802和 MSPM0 MCU 的双射线烟雾探测器应用手册中所述的红外 LED、蓝色 LED 和反射增量的预期变化 [演示 GUI -第10页],请给我一份正确的MSPM0L1306 -Launchpad和的硬件连接图示,能让我配合sdk_lp_mspm0l1306_demos_dualray_smoke_detector源代码运行,万分感谢

  • 您好,

    已经收到了您的案例,调查需要些时间,感谢您的耐心等待