Part Number: PGA460
I used command 05 to read measurement results, monitoring only one object, but the return value shows the first four bytes of command 07. What's going on? Both setting 0 and setting 1 for DATADUMP_EN return the first four bytes of command 07. Below is an example of the return value when setting 1:
The first part shows the response to command 05, followed by the response to command 07, both using a 300 kHz frequency.

This is the oscilloscope capture when sending command 5. Below is another screenshot of the oscilloscope capture when sending command 7. Hope this helps.