This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: IWR6843AOPEVM: XDS110 only enumerates Data Port, Application/User UART missing

Part Number: IWR6843AOPEVM

IWR6843AOPEVM: XDS110 only shows Data Port, Application/User UART missing on windows 10. 

Hello,
I am using an IWR6843AOPEVM EVM board (no booster board or carrier board attached). The board powers up normally and all LEDs turn on when connected to USB. I am using the micro‑USB port on the debugger side (the only one that lights the LEDs).

Issue:
Windows enumerates the XDS110 incorrectly. Under Ports (COM & LPT) I get:

  • XDS110 Class Data Port (COMxx)
  • XDS110 Class Data Port (COMxx)

The XDS110 Class Application/User UART does not appear at all.

Under Other Devices, I also see entries named “Standard COM Port” and “Enhanced COM Port” with yellow warning icons. None of the TI XDS110 drivers will bind to these ports.

Tools tried (all fail):

  • Installed the full XDS110 driver package
  • Manual driver binding (Debug Probe, CMSIS‑DAP, Serial Trace, Data Port)
  • xds110reset.exe → error: Failed to connect to XDS110 (-260)
  • xdsdfu -eFound 0 devices
  • Power-cycle, different cables, different USB ports
  • SOP jumper check (EVM powers and boots fine)

Symptoms summary:

  • Only the Data Port enumerates (twice)
  • Application/User UART endpoint never appears
  • XDS110 cannot be accessed by DFU or reset tools
  • Board powers normally and antennas/LEDs all behave
  • Drivers are present on the PC but debugger firmware is not exposing all interfaces

This appears to be a corrupted XDS110 firmware on the EVM’s onboard debugger, where only the Data Port interface is active and the Application/User UART is missing completely.

Could you please provide guidance on how to recover or reflash the XDS110 firmware on the IWR6843AOPEVM, or advise if the debugger section requires repair/replacement?