Part Number: LDC1001-Q1
1.对寄存器进行写命令时,在SDI可以检测到MCU写入的数据,但是SDO无回复数据。只有对寄存器进行读命令时才可以在SDO检测到回复数据,怎么样才能写入?
2.0x01,0x05,0x0B,使用命令写入后读取出的数据和写入的不符,可能的原因?
3.0x04,0x05,写入的时候会一起改变(写入一个但是读取两个两个的数据是一样的)。为什么会这样?
4.使用示波器探针测量时钟和SDI时,同时检测SDI写入数据和SDO读取数据时,数据同时变为0。SDO的数据为0,出现这种现象的原因?