This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: UART test demo problem ---- Can not receive signal from dss domain in PC serial port

Part Number: AWR1843BOOST

I tried uart/test for awr1843Boost  in SDK 3.1.0.2

Greatly, I can definitely receive UART signals from the MSS domain. There are TWO UARTs in MSS domain by the manifest, and both of them are working well. All test signals can be received in win10 platform using a serial assist software in baudrate 115200. 

I believe this means all the  configurations in MSS domain for two UARTs are correct.

However, no signals can be detected from DSS domain. Only ONE UART is available is DSS domain by the manifest.

There are two available PORT in my computer(PORT3 for UART and PORT4 for DATA), and NON of them can received any signal from DSS domain.

In the test code, the MSS domain will be suspended until the DSS domain finished. 

But no signal detected from DSS domain. Signals can only be detected from MSS domain after the DSS domain finished.

Hope some help.

baudrate: 115200

pinmux:

console output:

QUESTION:

There are some output in CCS debugging console from DSS domain(Start with [C674X_0]) and no error asserts while opening the UART in DSS domain.

1. IS the UART  opened ?

2. What should I do to make DSS domain UART work?