This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1101: 关于Rp值测量的疑问

Part Number: LDC1101


你好,铁氧体磁芯电感,丝包线绕制。26mm尺寸的电感,83uH,工作频率700Khz,零点到满量程Rp(3K~45K)。测距15mm。想用Rp+L的模式来测量。

现在单片机读这个Rp,近距离还可以,远距离之后,Rp跳动很大。

Q1:跳动这么大,有没有好办法解决。8mm之后,每mm跳动几百Ω。

感觉没法测了,我最终想要输出跟位移对应的模拟量,对他滤波太厉害,反应时间太慢~

Schematic_位移传感器_2021-07-09.pdf