This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: mmwave studio: Unable to read FPGA version. [error -5]

Part Number: DCA1000EVM
Other Parts Discussed in Thread: IWR6843

我按照https://www.ti.com/lit/ug/spruij4a/spruij4a.pdf的内容来刷新FPGA,上面的这一步要求Device和Package如此设定, ,但是我这里没有PDF里提到的这两个选项 ,Package也只有两个8pin的。请问我该怎么解决标题上的问题

  • 请问使用的Lattice Diamond programmer toold的版本是Programmer Standalone 3.10 64- bit for Windows吗?

  • PPT上给的这个地址www.latticesemi.com/programmer,里面只有3.12,如果用3.10就可以解决请您给个地址

  • 请联系Lattice公司看是否能提供3.10的版本。

  • 我不知道怎么联系。为什么会出现这种问题,其他人用DCA1000时不会出现这个问题吗,他们是怎么解决的

  • 下面是他们的技术支持网站。
    https://www.latticesemi.com/en/Support

  • 不是版本问题,我之前点错按钮了,我按照PDF的流程到LD14亮,中间用的文件是DCA1000_FPGA_RECORD_V2.8_05JUL2019.bit,再用mmwave studio, ,前面的蓝色按钮都点好了,再点set up DCA1000,点connect,reset and,然后还出现之前的那个错误.具体如下

    GM: Constructor
    GM: Wed Jul 28 17:16:10 2021
    RSTD.Transmit("/Settings")
    [17:16:11]
    [17:16:11] ### Running Startup script: "D:\Ti\mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Startup.lua" ###
    [17:16:11] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
    [17:16:11] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
    [17:16:11] Scripter ignored: Attempt to UnBuild() again or before Build.
    [17:16:11] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "D:\\Ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
    [17:16:11] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
    [17:16:11] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
    [17:16:11] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
    [17:16:11] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
    [17:16:11] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
    [17:16:11] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "D:\\Ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\RunTime\\SAL.dll")
    [17:16:11] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
    [17:16:11] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
    [17:16:11] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
    [17:16:11] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
    [17:16:11] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
    [17:16:11] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
    [17:16:11] RSTD.Transmit("/")
    [17:16:11] RSTD.SaveSettings(): Settings saved to "C:\Users\lenovo\AppData\Roaming\RSTD\config.xml"
    [17:16:11] RSTD.Build()
    [17:16:11] RSTD.SaveSettings(): Settings saved to "C:\Users\lenovo\AppData\Roaming\RSTD\config.xml"
    [17:16:11] RSTD.Transmit("/")
    [17:16:11] RSTD.AL_Build()
    [17:16:11] RSTD.AL_LoadXml()
    [17:16:11] RSTD.Transmit("/")
    [17:16:11] RSTD.AL_Init()
    [17:16:11] RSTD.Clients_Build()
    [17:16:11] GM: Init
    [17:16:11] GM: Loaded 'D:\Ti\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\\LabClient.dll'
    [17:16:11] GM: 1 Guest (s) init
    [17:16:11] GM: 1 Module(s) init
    [17:16:11] GM: 2 Tab (s) init
    [17:16:11] RSTD.Client_LoadXml()
    [17:16:11] [RadarAPI]: ar1.selectRadarMode(0)
    [17:16:11] [RadarAPI]: Status: Passed
    [17:16:11] Matlab Runtime Engine is installed
    [17:16:11] [RadarAPI]: Starting Matlab Engine..
    [17:16:17] [RadarAPI]: Matlab Engine Started!
    [17:16:19] [RadarAPI]: ar1.selectCascadeMode(0)
    [17:16:19] [RadarAPI]: Status: Passed
    [17:16:19] [RadarAPI]: ar1.LoadSettings('C:\Users\lenovo\AppData\Roaming\RSTD\ar1gui.ini')
    [17:16:19] TESTING = false
    [17:16:19] RstdNet: Port 2777: Listening..
    [17:16:19]
    [17:16:19] ***Script completed successfully.***
    [17:18:37] [RadarAPI]: Opening Gpio Control Port()
    [17:18:37] [RadarAPI]: Status: Passed
    [17:18:38] [RadarAPI]: Opening Board Control Port()
    [17:18:38] [RadarAPI]: Status: Passed
    [17:18:39] [RadarAPI]: ar1.FullReset()
    [17:18:39] [RadarAPI]: Status: Passed
    [17:18:39] [RadarAPI]: Closing Board Control Port()
    [17:18:39] [RadarAPI]: Status: Passed
    [17:18:39] [RadarAPI]: Closing Gpio Control Port()
    [17:18:39] [RadarAPI]: Status: Passed
    [17:18:39] [RadarAPI]: ar1.SOPControl(2)
    [17:18:39] [RadarAPI]: Status: Passed
    [17:18:40] [RadarAPI]: ar1.Connect(7,115200,1000)
    [17:18:41] [RadarAPI]: ar1.Calling_IsConnected()
    [17:18:42] [RadarAPI]: ar1.SelectChipVersion("IWR6843")
    [17:18:42] [RadarAPI]: Status: Passed
    [17:18:42] [RadarAPI]: ar1.frequencyBandSelection("60G")
    [17:18:42] [RadarAPI]: ar1.SelectChipVersion("IWR6843")
    [17:18:42] [RadarAPI]: Status: Passed
    [17:18:42] Device Status : IWR6843/QM/SOP:2/ES:2
    [17:18:42] [RadarAPI]: ar1.SaveSettings('C:\Users\lenovo\AppData\Roaming\RSTD\ar1gui.ini')
    [17:18:45] [RadarAPI]: ar1.DownloadBSSFw("D:\\Ti\\mmwave_studio_02_01_01_00\\rf_eval_firmware\\radarss\\xwr68xx_radarss.bin")
    [17:18:45] [RadarAPI]: Downloading BSS ROM RPRC Binary..
    [17:19:33] [RadarAPI]: ar1.GetBSSFwVersion()
    [17:19:33] [RadarAPI]: BSSFwVersion:(06.02.01.05 (09/03/20))
    [17:19:33] [RadarAPI]: ar1.DownloadMSSFw("D:\\Ti\\mmwave_studio_02_01_01_00\\rf_eval_firmware\\masterss\\xwr68xx_masterss.bin")
    [17:19:34] [RadarAPI]: Downloading MSS RPRC Binary..
    [17:19:53] [RadarAPI]: ar1.GetMSSFwVersion()
    [17:19:53] [RadarAPI]: MSSFwVersion:(02.00.00.03 (27/08/19))
    [17:20:00] [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
    [17:20:00] [RadarAPI]: Status: Passed
    [17:20:00] MSS power up done async event received!
    [17:20:02] [RadarAPI]: ar1.SelectChipVersion("IWR6843")
    [17:20:02] [RadarAPI]: Status: Passed
    [17:20:02] [RadarAPI]: ar1.SelectChipVersion("IWR6843")
    [17:20:02] [RadarAPI]: Status: Passed
    [17:20:02] Device Status : IWR6843/QM/SOP:2/ES:2
    [17:20:02] [RadarAPI]: ar1.RfEnable()
    [17:20:02] BSS power up done async event received!
    [17:20:02] [RadarAPI]: Status: Passed
    [17:20:03] [RadarAPI]: ar1.GetMSSFwVersion()
    [17:20:03] [RadarAPI]: MSSFwVersion:(02.00.00.03 (27/08/19))
    [17:20:03] [RadarAPI]: ar1.GetBSSFwVersion()
    [17:20:03] [RadarAPI]: BSSFwVersion:(06.02.01.05 (09/03/20))
    [17:20:08] [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
    [17:20:08] [RadarAPI]: Status: Passed
    [17:20:11] [RadarAPI]: ar1.LPModConfig(0, 0)
    [17:20:11] [RadarAPI]: Status: Passed
    [17:20:11] [RadarAPI]: ar1.RfInit()
    [17:20:11] RF Init async event received!
    [17:20:11] [RadarAPI]: Status: Passed
    [17:20:11] [RadarAPI]: Time stamp, Temperture: 8790,52; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 1, 1; RxIQMM Status, Update: 1, 1;
    [17:20:14] [RadarAPI]: ar1.DataPathConfig(513, 1216644097, 0)
    [17:20:14] [RadarAPI]: Status: Passed
    [17:20:15] [RadarAPI]: ar1.LvdsClkConfig(1, 1)
    [17:20:15] [RadarAPI]: Status: Passed
    [17:20:16] [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0)
    [17:20:16] [RadarAPI]: Status: Passed
    [17:20:20] [RadarAPI]: ar1.ProfileConfig(0, 60, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 10000, 0, 131072, 30)
    [17:20:20] [RadarAPI]: Status: Passed
    [17:20:22] [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 0, 0)
    [17:20:22] [RadarAPI]: Status: Passed
    [17:20:22] Test Source Already Disabled...!!!
    [17:20:22] [RadarAPI]: ar1.DisableTestSource(0)
    [17:20:22] [RadarAPI]: Status: Passed
    [17:20:22] [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 0, 1)
    [17:20:23] [RadarAPI]: Status: Passed
    [17:20:23] [RadarAPI]: ar1.GetCaptureCardDllVersion()
    [17:20:23] [RadarAPI]: Sending dll_version command to DCA1000
    [17:20:23] [RadarAPI]:
    [17:20:23] DLL Version : 1.0
    [17:20:23] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
    [17:20:23] [RadarAPI]: Status: Passed
    [17:21:41] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
    [17:21:41] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30)
    [17:21:41] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
    [17:21:41] [RadarAPI]: Sending fpga command to DCA1000
    [17:21:51] [RadarAPI]:
    [17:21:51] FPGA Configuration :
    [17:21:51] Timeout Error! System disconnected
    [17:21:51] [RadarAPI]: Sending record command to DCA1000
    [17:22:01] [RadarAPI]:
    [17:22:01] Configure Record :
    [17:22:01] Timeout Error! System disconnected
    [17:22:01] [RadarAPI]: ar1.GetCaptureCardFPGAVersion()
    [17:22:01] [RadarAPI]: Sending fpga_version command to DCA1000
    [17:22:11] [RadarAPI]:
    [17:22:11]
    [17:22:11] Unable to read FPGA Version. [error -5]
    [17:22:11]

  • PDF指的是https://www.ti.com/lit/ug/spruij4a/spruij4a.pdf  中的9  FPGA Programming .......................................... 22

  • 已经解决了。是防火墙的问题。把Windows Defender 防火墙的来宾或公用网络关了即可。如图

  • 感谢分享!