This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP175: TMP175 驱动问题

Part Number: TMP175
Other Parts Discussed in Thread: TMP75, TMP421, , TMP102, TMP401

你好!

     我们目前使用TMP75,采用和LM75兼容的驱动。LM75代码在内核中是SMBus,非I2c驱动。目前LM75跟TP挂到同一路I2c,从log来看I2C被占用,怀疑SMBus跟I2c不能同时使用,是否可以提供LM75  I2c的驱动?详细log如附件,请参考!

err_kernel_log.docx

  • 您好,我这边看了下,很抱歉我们没有LMP175的code可以参考。但是您可以参考Linux Kernel的关于TMP421,401和102这几款的C code,然后可以针对TMP175的寄存器做一些修改。

    https://www.kernel.org/ 下载最新版本Kernel,然后安装路径下应该是有这几款的.c 文件。比如:

    \linux-3.16.1.tar\linux-3.16.1\drivers\hwmon\tmp102.c or tmp401.c or tmp421.c