This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
老师您好,我有一个问题想请教一下:我在SenSorConfig当中的 Frame 模块中设置的Periodicity为60ms,每个frame设置128个chirp,总共设置1000帧,如图所示:
这意味着我即将在1分钟内发送1000x128=128000个chirp. 现在我设置对于每一个chirp采250个点,采样率为5Msps,如图所示:,这是不是意味着我在1分钟内发的所有chirp即将在(128000x250)/5e6=6.4秒内完成啊?
嗯嗯。老师您好,我还有一个问题:如上面设置,最终我采集到的数据从时域上看就6.4秒。如果反过来我想增加时域上的观察时间例如为30s,这就意味着我要增加发送的frames,但是如果增加发送的frames,我对应的数据量就会很大,在做一些处理的时候,可能会导致内存不足。于是我想通过降低采样率来缓解一下这个问题,当我降低采样率的时候,会出现如图所示的问题:,这是什么原因啊?
请尝试用 mmwave sudio->RampTimingCalculator 计算一下ramp end time参数。请参考下面的文档5.4 Example Timing Calculation Using the Calculator
https://www.ti.com/cn/lit/an/swra553a/swra553a.pdf