This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: 关于使用mmWave Studio 对IWR1843BOOST配置的相关问题

Part Number: IWR1843BOOST


老师您好,我有一个问题想请教一下:我在SenSorConfig当中的 Frame 模块中设置的Periodicity为60ms,每个frame设置128个chirp,总共设置1000帧,如图所示:

这意味着我即将在1分钟内发送1000x128=128000个chirp. 现在我设置对于每一个chirp采250个点,采样率为5Msps,如图所示: ,这是不是意味着我在1分钟内发的所有chirp即将在(128000x250)/5e6=6.4秒内完成啊?