Other Parts Discussed in Thread: DCA1000EVM, AWR2243, AWR1243
用mmwavelink_example来配置雷达,采集雷达数据,得到的数据大小不对。
相同的配置下比用mmWave studio采集的数据量少一半。
我使用3发4收的雷达,采样点数为173,chirpLoops数为101,帧数为960,数据格式采用complex 1x(16bits)
理论上采集的数据大小应该是:3*4*173*101*960*4 bytes = 805 155 840 bytes
但是实际只采集到402 577 920 bytes的数据,更好是理论的一半。
请问能帮忙看一下,我配置中哪里出了问题?以下是mmwaveconfig.txt和DCA1000EVM_CLI的一些关键配置。
#3t4r #For detailed view of mmWave Radar configuration structure #please refer #ti\control\mmwavelink\docs\doxygen\html\index.html # # #Global configuration #Advanced frame test enable/disable; 1 - Advanced frame; 0 - Legacy frame #Continuous mode test enable/disable; 1 - Enable; 0 - Disable #Dynamic chirp test enable/disable; 1 - Enable; 0 - Disable; This should not be enabled if Advanced chirp test is enabled #Dynamic profile test enable/disable; 1 - Enable; 0 - Disable #Advanced chirp test enable/disable; 1 - Enable; 0 - Disable; The legacy chirp API is not required if this is enabled #Firmware download enable/disable; 1 - Enable; 0 - Disable #mmWaveLink logging enable/disable; 1 - Enable; 0 - Disable #Calibration enable/disable; To perform calibration store/restore; 1 - Enable; 0 - Disable #Calibration Store/Restore; If CalibEnable = 1, then whether to store/restore; 1 - Store; 0 - Restore #Transport mode; 1 - I2C; 0 - SPI #Flash connected enable/disable; 1 - Enable; 0 - Disable # # 是否启用高级帧 LinkAdvanceFrameTest=0; LinkContModeTest=0; LinkDynProfileTest=0; LinkDynChirpTest=0; LinkAdvChirpTest=0; EnableFwDownload=1; # 日志 EnableMmwlLogging=1; # 是否校准 CalibEnable=0; CalibStoreRestore=1; # 传输模式 SPI TransferMode=0; IsFlashConnected=1; #END # #power on master arguments, please modify if needed. #rlClientCbs_t: crcType 0:16Bit/1:32Bit/2:64Bit, ackTimeout # crcType=1; ackTimeout=1000; #END # #channel config parameters, please modify if needed. #rlChanCfg_t 通道配置 channelTx=7; channelRx=15; # 级联模式 cascading=0; #END # #ADC out config parameters, please modify if needed. #rlAdcOutCfg_t #0-12bits; 1-14bits; 2-16bits adcBits=2; # 0-real; 1-Complex 1x;2-Complex 2x adcFormat=1; #END # #DATA format config parameters, please modify if needed. #rlDevDataFmtCfg_t #0b1111-四收 rxChanEn=15; # 0-12bits;1-14bits;2-16bits adcBitsD=2; # 0-real;1-Complex 1x;2-Complex 2x adcFmt=1; # 0-I first;1-Q first iqSwapSel=0; # 0交错模式 chInterleave=0; #END # #Low power config Paramters, please modify if needed. #rlLowPowerModeCfg_t 未知 ############ # anaCfg=0; lpAdcMode=0; #END # #Data Path config parameters, please modify if needed # 0-CSI2; 1-LVDS intfSel=1; transferFmtPkt0=1; transferFmtPkt1=0; cqConfig=2; cq0TransSize=64; cq1TransSize=64; cq2TransSize=64; #END # #LVDS clock config parameters, please modify if needed #rlDevDataPathClkCfg_t # 时钟类型 0 SDR; 1 DDR laneClk=1; dataRate=1; #END # #SET HSI clock parameters, please modify if needed. #rlDevHsiClk_t 未知 ############ # hsiClk=9 #END # #LANE config parameters, please modify if needed. #rlDevLaneEnable_t # 0b1111 四个通道 # laneEn=15; #END # #LVDS Lane Config parameters, please modify if needed. #rlDevLvdsLaneCfg_t 未知 ############ # laneFmtMap=0; laneParamCfg=1; #END # #Programmable Filter config parameters, please modify if needed. #rlRfProgFiltConf_t 未知作用###### # profileId=0; coeffStartIdx=0; progFiltLen=14; progFiltFreqShift=100; #END # #Profile config parameters, please modify if needed. #rlProfileCfg_t # profileId=0; pfVcoSelect=2; startFreqConst=1435384036; idleTimeConst=300; adcStartTimeConst=420; rampEndTime=2122; txOutPowerBackoffCode=0; txPhaseShifter=0; freqSlopeConst=593; txStartTime=100; numAdcSamples=173; digOutSampleRate=10604; hpfCornerFreq1=0; hpfCornerFreq2=0; rxGain=30; #END # #Chirp Configuration parameters, please modify if needed. #rlChirpCfg_t # chirpStartIdx=0; chirpEndIdx=0; profileIdCPCFG=0; startFreqVar=0; freqSlopeVar=0; idleTimeVar=0; adcStartTimeVar=0; # 0b0001 txEnable=1; #END # #Chirp Configuration parameters, please modify if needed. #rlChirpCfg_t # chirpStartIdx=1; chirpEndIdx=1; profileIdCPCFG=0; startFreqVar=0; freqSlopeVar=0; idleTimeVar=0; adcStartTimeVar=0; # 0b0100 txEnable=4; #END # #Chirp Configuration parameters, please modify if needed. #rlChirpCfg_t # chirpStartIdx=2; chirpEndIdx=2; profileIdCPCFG=0; startFreqVar=0; freqSlopeVar=0; idleTimeVar=0; adcStartTimeVar=0; # 0b0010 txEnable=2; #END # #Frame configuration parameters, please modify if needed. #rlFrameCfg_t # chirpStartIdxFCF=0; chirpEndIdxFCF=2; frameCount=960; loopCount=101; periodicity=12500000; triggerDelay=0; numAdcSamples=173; # 软件触发 triggerSelect=1; #END
{
"DCA1000Config": {
"dataLoggingMode": "multi",
"dataTransferMode": "LVDSCapture",
"dataCaptureMode": "ethernetStream",
"lvdsMode": 1,
"dataFormatMode": 3,
"packetDelay_us": 25,
"ethernetConfig": {
"DCA1000IPAddress": "192.168.33.180",
"DCA1000ConfigPort": 4096,
"DCA1000DataPort": 4098
},
"ethernetConfigUpdate": {
"systemIPAddress": "192.168.33.30",
"DCA1000IPAddress": "192.168.33.181",
"DCA1000MACAddress": "12.34.56.78.90.12",
"DCA1000ConfigPort": 4096,
"DCA1000DataPort": 4098,
},
"captureConfig": {
"fileBasePath": "D:\\RadarData\\cmd",
"filePrefix": "adc_data",
"maxRecFileSize_MB": 1024,
"sequenceNumberEnable": 1,
"captureStopMode": "frames",
"framesToCapture": 960
},
"dataFormatConfig": {
"MSBToggle": 1,
"reorderEnable": 1,
"laneFmtMap": 3,
"dataPortConfig": [
{
"portIdx": 0,
"dataType": "complex"
},
{
"portIdx": 1,
"dataType": "complex"
},
{
"portIdx": 2,
"dataType": "complex"
},
{
"portIdx": 3,
"dataType": "complex"
},
{
"portIdx": 4,
"dataType": "complex"
}
]
}
}
}