This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: 使用mmWaveStudio采集数据时出现【Error : The number of files captured is zero!】

Part Number: AWR1642


我按照DCA1000EVM Quick Start Guide (ti.com)上面的步骤进行数据采集,但遇到了“Error : The number of files captured is zero!”的问题,如下图所示

我使用的是5V3A的电源。

电脑的防火墙已经关闭。

按照.《DCA1000 Debugging Handbook》上的教程排查了如下问题

但最终仍然没有解决。
恳请您指导我一下该如何解决这个问题。
期待您的答复!

【以下是我在采集过程中的相关信息】

①mmwaveStudio的所有输出如下,Error : The number of files captured is zero!”出现在最后一行。

GM: Constructor
GM: Tue Dec 07 11:11:43 2021
RSTD.Transmit("/Settings")
[11:11:43]  
[11:11:43]  ### Running Startup script: "C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Startup.lua" ###
[11:11:43]  RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[11:11:43]  RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[11:11:43]  Scripter ignored: Attempt to UnBuild() again or before Build.
[11:11:43]  RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[11:11:43]  RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[11:11:43]  RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[11:11:43]  RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[11:11:43]  RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[11:11:43]  RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[11:11:43]  RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\RunTime\\SAL.dll")
[11:11:43]  RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[11:11:43]  RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[11:11:43]  RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[11:11:43]  RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[11:11:43]  RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[11:11:43]  RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
[11:11:43]  RSTD.Transmit("/")
[11:11:43]  RSTD.SaveSettings(): Settings saved to "C:\Users\LNN\AppData\Roaming\RSTD\config.xml"
[11:11:43]  RSTD.Build()
[11:11:43]  RSTD.SaveSettings(): Settings saved to "C:\Users\LNN\AppData\Roaming\RSTD\config.xml"
[11:11:43]  RSTD.Transmit("/")
[11:11:43]  RSTD.AL_Build()
[11:11:43]  RSTD.AL_LoadXml()
[11:11:43]  RSTD.Transmit("/")
[11:11:43]  RSTD.AL_Init()
[11:11:43]  RSTD.Clients_Build()
[11:11:43]  GM: Init
[11:11:43]  GM: Loaded 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\\LabClient.dll'
[11:11:43]  GM: 1 Guest (s) init
[11:11:43]  GM: 1 Module(s) init
[11:11:43]  GM: 2 Tab   (s) init
[11:11:43]  RSTD.Client_LoadXml()
[11:11:43]  [RadarAPI]: ar1.selectRadarMode(0)
[11:11:44]  [RadarAPI]: Status: Passed
[11:11:44]  Matlab Runtime Engine is installed
[11:11:44]  [RadarAPI]: Starting Matlab Engine..
[11:11:47]  [RadarAPI]: Matlab Engine Started!
[11:11:48]  [RadarAPI]: ar1.selectCascadeMode(0)
[11:11:48]  [RadarAPI]: Status: Passed
[11:11:48]  [RadarAPI]: ar1.LoadSettings('C:\Users\LNN\AppData\Roaming\RSTD\ar1gui.ini')
[11:11:49]  TESTING = false
[11:11:49]  RstdNet: Port 2777: Listening..
[11:11:49]  
[11:11:49]  ***Script completed successfully.***
[11:11:56]  [RadarAPI]: Opening Gpio Control Port()
[11:11:56]  [RadarAPI]: Status: Passed
[11:11:56]  [RadarAPI]: Opening Board Control Port()
[11:11:56]  [RadarAPI]: Status: Passed
[11:11:57]  [RadarAPI]: ar1.FullReset()
[11:11:57]  [RadarAPI]: Status: Passed
[11:11:58]  [RadarAPI]: Closing Board Control Port()
[11:11:58]  [RadarAPI]: Status: Passed
[11:11:58]  [RadarAPI]: Closing Gpio Control Port()
[11:11:58]  [RadarAPI]: Status: Passed
[11:11:58]  [RadarAPI]: ar1.SOPControl(2)
[11:11:58]  [RadarAPI]: Status: Passed
[11:11:59]  [RadarAPI]: ar1.Connect(7,921600,1000)
[11:12:02]  [RadarAPI]: Warning: Connected with baudrate 115200
[11:12:03]  [RadarAPI]: Warning: Disconnected existing BaudRate
[11:12:03]  [RadarAPI]: Warning: Trying to connect with baudrate 921600
[11:12:04]  [RadarAPI]: ar1.Calling_IsConnected()
[11:12:06]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
[11:12:06]  [RadarAPI]: Status: Passed
[11:12:06]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
[11:12:06]  [RadarAPI]: Status: Passed
[11:12:06]  [RadarAPI]: ar1.deviceVariantSelection("XWR1642")
[11:12:06]  [RadarAPI]: Status: Passed
[11:12:06]  [RadarAPI]: ar1.frequencyBandSelection("77G")
[11:12:06]  [RadarAPI]: ar1.SelectChipVersion("XWR1642")
[11:12:06]  [RadarAPI]: Status: Passed
[11:12:06]  Device Status : XWR1642/QM/SOP:2/ES:2
[11:12:06]  [RadarAPI]: ar1.SaveSettings('C:\Users\LNN\AppData\Roaming\RSTD\ar1gui.ini')
[11:12:08]  [RadarAPI]: ar1.ReadRegister(0xffffe214, 0, 31)
[11:12:08]  [RadarAPI]: ar1.ReadRegister(0xffffe210, 0, 31)
[11:12:08]  [RadarAPI]: ar1.ReadRegister(0xffffe218, 0, 31)
[11:12:08]  [RadarAPI]: ar1.DownloadBSSFw("C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\radarss\\xwr16xx_radarss.bin")
[11:12:09]  [RadarAPI]: Downloading BSS Patch RPRC Binary..
[11:12:11]  [RadarAPI]: ar1.GetBSSFwVersion()
[11:12:11]  [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))
[11:12:11]  [RadarAPI]: ar1.GetBSSPatchFwVersion()
[11:12:11]  [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19))
[11:12:11]  BSS FW Download Success
[11:12:11]  [RadarAPI]: ar1.DownloadMSSFw("C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Scripts\\..\\..\\rf_eval_firmware\\masterss\\xwr16xx_masterss.bin")
[11:12:12]  [RadarAPI]: Downloading MSS RPRC Binary..
[11:12:14]  [RadarAPI]: ar1.GetMSSFwVersion()
[11:12:14]  [RadarAPI]: MSSFwVersion:(01.02.05.02 (16/07/19))
[11:12:14]  MSS FW Download Success
[11:12:15]  [RadarAPI]: ar1.PowerOn(0, 1000, 0, 0)
[11:12:15]  MSS power up done async event received!
[11:12:15]  [RadarAPI]: Status: Passed
[11:12:15]  Power On Success
[11:12:15]  [RadarAPI]: ar1.SelectChipVersion("AR1642")
[11:12:15]  [RadarAPI]: Status: Passed
[11:12:15]  [RadarAPI]: ar1.SelectChipVersion("XWR1642")
[11:12:15]  [RadarAPI]: Status: Passed
[11:12:16]  Device Status : XWR1642/QM/SOP:2/ES:2
[11:12:16]  [RadarAPI]: ar1.RfEnable()
[11:12:16]  BSS power up done async event received!
[11:12:16]  [RadarAPI]: Status: Passed
[11:12:16]  [RadarAPI]: ar1.GetMSSFwVersion()
[11:12:16]  [RadarAPI]: MSSFwVersion:(01.02.05.02 (16/07/19))
[11:12:17]  [RadarAPI]: ar1.GetBSSFwVersion()
[11:12:17]  [RadarAPI]: BSSFwVersion:(02.00.00.01 (05/10/17))
[11:12:17]  [RadarAPI]: ar1.GetBSSPatchFwVersion()
[11:12:17]  [RadarAPI]: BSSPatchFwVersion:(01.02.05.02 (30/04/19))
[11:12:17]  RF Enable Success
[11:12:18]  [RadarAPI]: ar1.ChanNAdcConfig(1, 1, 0, 1, 1, 1, 1, 2, 1, 0)
[11:12:18]  [RadarAPI]: Status: Passed
[11:12:18]  ChanNAdcConfig Success
[11:12:18]  [RadarAPI]: ar1.LPModConfig(0, 1)
[11:12:18]  [RadarAPI]: Status: Passed
[11:12:18]  LPModConfig Success
[11:12:18]  [RadarAPI]: ar1.RfInit()
[11:12:18]  RF Init async event received!
[11:12:18]  [RadarAPI]: Time stamp, Temperture: 2182,30; APLL Status, Update: 1, 0; SynthVCO1 Status, Update: 1, 1; SynthVCO2 Status, Update: 1, 1; LODist Status, Update: 1, 1; RxADCDC Status, Update: 1, 1; HPFcutoff Status, Update: 1, 1; LPFcutoff Status, Update: 1, 1; PeakDetector Status, Update: 1, 1; TxPower Status, Update: 1, 1; RxGain Status, Update: 1, 1; TxPhase Status, Update: 0, 0; RxIQMM Status, Update: 1, 1; 
[11:12:18]  [RadarAPI]: Status: Passed
[11:12:18]  RfInit Success
[11:12:19]  [RadarAPI]: ar1.DataPathConfig(1, 1, 0)
[11:12:19]  [RadarAPI]: Status: Passed
[11:12:19]  DataPathConfig Success
[11:12:19]  [RadarAPI]: ar1.LvdsClkConfig(1, 1)
[11:12:19]  [RadarAPI]: Status: Passed
[11:12:19]  LvdsClkConfig Success
[11:12:19]  [RadarAPI]: ar1.LVDSLaneConfig(0, 1, 1, 0, 0, 1, 0, 0)
[11:12:19]  [RadarAPI]: Status: Passed
[11:12:19]  LVDSLaneConfig Success
[11:12:19]  [RadarAPI]: ar1.SetTestSource(4, 3, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0)
[11:12:19]  [RadarAPI]: Status: Passed
[11:12:19]  Test Source Configuration Success
[11:12:19]  [RadarAPI]: ar1.ProfileConfig(0, 77, 100, 6, 60, 0, 0, 0, 0, 0, 0, 29.982, 0, 256, 5000, 0, 0, 30)
[11:12:19]  [RadarAPI]: Status: Passed
[11:12:19]  ProfileConfig Success
[11:12:19]  [RadarAPI]: ar1.ChirpConfig(0, 0, 0, 0, 0, 0, 0, 1, 1, 0)
[11:12:19]  [RadarAPI]: Status: Passed
[11:12:19]  ChirpConfig Success
[11:12:19]  [RadarAPI]: ar1.EnableTestSource(1)
[11:12:20]  [RadarAPI]: Status: Passed
[11:12:20]  Enabling Test Source Success
[11:12:20]  Test Source Already Enabled...!!!
[11:12:20]  [RadarAPI]: ar1.EnableTestSource(1)
[11:12:20]  [RadarAPI]: Status: Passed
[11:12:20]  [RadarAPI]: ar1.FrameConfig(0, 0, 8, 128, 40, 0, 0, 1)
[11:12:20]  [RadarAPI]: Status: Passed
[11:12:20]  FrameConfig Success
[11:12:20]  [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[11:12:20]  [RadarAPI]: Status: Passed
[11:12:20]  SelectCaptureDevice Success
[11:12:20]  [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "c:22:38:4e:5a:c", 4096, 4098)
[11:12:20]  [RadarAPI]: Sending fpga command to DCA1000
[11:12:20]  [RadarAPI]: 
[11:12:20]  FPGA Configuration command : Success
[11:12:20]  [RadarAPI]: Sending fpga_version command to DCA1000
[11:12:20]  [RadarAPI]: 
[11:12:20]  
[11:12:20]  FPGA Version : 2.7 [Record]
[11:12:20]  
[11:12:20]  CaptureCardConfig_EthInit Success
[11:12:20]  [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 0)
[11:12:20]  [RadarAPI]: Sending fpga command to DCA1000
[11:12:20]  [RadarAPI]: 
[11:12:20]  FPGA Configuration command : Success
[11:12:20]  CaptureCardConfig_Mode Success
[11:12:20]  [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
[11:12:20]  [RadarAPI]: Sending fpga command to DCA1000
[11:12:20]  [RadarAPI]: 
[11:12:20]  FPGA Configuration command : Success
[11:12:20]  [RadarAPI]: Sending record command to DCA1000
[11:12:20]  [RadarAPI]: 
[11:12:20]  Configure Record command : Success
[11:12:20]  CaptureCardConfig_PacketDelay Success
[11:12:21]  [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin", 1)
[11:12:21]  [RadarAPI]: Sending start_record command to DCA1000
[11:12:21]  [RadarAPI]: Status: Passed
[11:12:22]  [RadarAPI]: ar1.StartFrame()
[11:12:22]  [RadarAPI]: Status: Passed
[11:12:22]  Frame start async event received!
[11:12:22]  Frame End async event received!
[11:12:22]  [RadarAPI]: Frame Ended
[11:12:27]  Please wait for a few seconds for matlab post processing .....!!!! 
[11:12:27]  [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Scripts\\..\\PostProc\\adc_data.bin")
[11:12:27]  [RadarAPI]: No of files Captured: 0, Total no of frames for each device : 8
[11:12:27]  Error : The number of files captured is zero!

②使用wireshark获取的数据包如下