This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR6843ISK: AWR6843isk 改变角度 FFT bin 大小 64 ->128

Part Number: AWR6843ISK

您好

      请问下在工业包里的 longe range people detection的lab 里,可以改变 angle fft 的bin size 吗?
默认是64,我想改成 128 或 256的话除了把aoapocdsp.h 里 #define DPU_AOAPROCDSP_NUM_ANGLE_BINS          (64U)

改成#define DPU_AOAPROCDSP_NUM_ANGLE_BINS          (128U),有其他地方需要设定吗?z我的主要目的是想要提高。

改完后我有重新build aoaproc 的library,载入到硬体后发生 下图错误情况,请问是什么原因呢?

角度量测精度。

sdk 版本:mmwave_sdk_03_05_00_04

软体 :C:\ti\mmwave_industrial_toolbox_4_7_0\labs\long_range_people_detection\68xx_long_range_people_det

硬体:AWR6843isk

谢谢!