Other Parts Discussed in Thread: AM2732, UNIFLASH, AWR2944EVM
您好,
当前运行MMWAVE SDK OOB Demo with Ethernet Streaming时,在python脚本中报错、没有目标数据输出,在MMWAVE Demo Visualizer中LOAD profile_enet.cfg也没有目标输出,似乎配置参数没有Load 进去,我的配置如下“
1)、固件刷录am273x_mmw_demoTDMEnet.appimage
2)、连接MMWAVE Demo Visualizer,通过queryLocalIP获取IP为Local IP is: 169.254.243.236
3)、更改以太网IP为169.254.243.237,修改tcpserver.py中HOST = '169.254.243.236' # Local IP Address
4)、运行tcpserver.py会出现如下错误
Python 3.10.2 (tags/v3.10.2:a58ebcc, Jan 17 2022, 14:12:15) [MSC v.1929 64 bit (AMD64)] on win32
Type "help", "copyright", "credits" or "license()" for more information.
= RESTART: E:\ti\mmwave_mcuplus_sdk_04_02_00_02\mmwave_mcuplus_sdk_04_02_00_02\ti\demo\utils\tcpserver.py
Traceback (most recent call last):
File "E:\ti\mmwave_mcuplus_sdk_04_02_00_02\mmwave_mcuplus_sdk_04_02_00_02\ti\demo\utils\tcpserver.py", line 61, in <module>
s.bind((HOST, PORT))
OSError: [WinError 10049] 在其上下文中,该请求的地址无效。
5)、修改profile_enet.cfg里面enetStreamCfg 1 169 254 243 237,在MMWAVE Demo Visualizer中LOAD profile_enet.cfg后无目标输出,如下:

麻烦帮忙看下如上配置是否有误,如何正确通过以太网获取相关数据。
谢谢。