This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT101: 将放大率降低的情况下, 是否会损失输出精度.

Part Number: OPT101


如果芯片供电是30V(Vs=30V),  假设光波长是850nm,   假设光接收器收到的光能量Radiant Power (μW)是 3uW, 此时经过调节外部电阻调整放大倍数, 使得此时的输出电压是10V, 存在正负0.1V波动.

如果此时芯片供电降低到1/10, 放大倍数也降低为1/10, 输出也会降低到1/10, 输出精度会如何变化?

也就是说, 芯片供电是3V(Vs=3V),  假设光波长是850nm,   假设光接收器收到的光能量Radiant Power (μW)仍旧是 3uW, 此时经过调节外部电阻调整放大倍数也降低到1/10, 使得此时的输出电压是1V,  那么此时电压是正负0.1V波动呢? 还是在0.01V波动?

  • 您好,

    您应该是指在不同供电电压和反馈电阻下的Nonlinearity,数据表给出的+/- 0.01 % of FS是在供电电压VS = 2.7V to 36V,反馈电阻为1MΩ时的一个典型值。很抱歉,我没有找到在其他反馈电阻下的线性度参数。

    另外请注意,数据表的线性性能部分还有一些附加信息,如下截图,即“对于小于100-μA的光电二极管电流,非线性保持在约0.05%以下。光电二极管能够在高辐射功率下产生1 mA或更大的输出电流,但在该区域非线性增加到几个百分点。”