This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA900: OWI can't activate PGA900

Part Number: PGA900


Hello,

Today , I had a problem,

OWI can't activate  PGA900

the High voltage is 6.5V

the Low voltage is 5V

when I change the VDD  from 5V  to 6.5V then 5V ,but can't activate the IC。

who  are kind enough to help?

thanks and best regards

Kim