已经配置好了参数脚本,代码如下:
--[[
Sequence being followed
A. CONFIGURATION
1. Connecting to TDA
1. Configuring Master from SOP till Channel Config
2. Configuring Slave (i) sequentially from SOP till SPI Connect. i = 1, 2, 3
3. Configuring Slaves together from F/W download till Channel Config
4. Configuring all devices together from LDO Bypass till Frame Config
NOTE:
Update the following in the script accordingly before running
1. metaImage F/W path on line 32
2. TDA Host Board IP Address on line 39
--]]
----------------------------------------User Constants--------------------------------------------
dev_list = {1, 2, 4, 8} -- Device map
RadarDevice = {1, 0, 0, 0} -- {dev1, dev2, dev3, dev4}, 1: Enable, 0: Disable
cascade_mode_list = {0, 2, 2, 2} -- 0: Single chip, 1: Master, 2: Slave
-- F/W Download Path
-- Uncomment the next line if you wish to pop-up a dialog box to select the firmware image file
-- Otherwise, hardcode the path to the firmware metaimage below
-- By default, the firmware filename is: xwr22xx_metaImage.bin
-- metaImagePath = RSTD.BrowseForFile(RSTD.GetSettingsPath(), "bin", "Browse to .bin file")
-- For 2243 ES1.1 devices
metaImagePath = "D:\\ti\\mmwave_dfp_02_02_03_01\\firmware\\xwr22xx_metaImage.bin"
-- For 2243 ES1.0 devices
-- metaImagePath = "D:\\ti\\mmwave_dfp_02_03_00_01\\firmware\\xwr22xx_metaImage.bin"
-- IP Address for the TDA2 Host Board
-- Change this accordingly for your setup
TDA_IPAddress = "192.168.33.180"
-- Device map of all the devices to be enabled by TDA
-- 1 - master ; 2- slave1 ; 4 - slave2 ; 8 - slave3
deviceMapOverall = RadarDevice[1] + (RadarDevice[2]*2) + (RadarDevice[3]*4) + (RadarDevice[4]*8)
deviceMapSlaves = (RadarDevice[2]*2) + (RadarDevice[3]*4) + (RadarDevice[4]*8)
-- Enable/Disable Test Source
-- This is useful during bringup
test_source_enable = 0 -- 0: Disable, 1: Enable
------------------------------------------- Sensor Configuration ------------------------------------------------
--[[
The sensor configuration consists of 3 sections:
1) Profile Configuration (common to all 4 AWR devices)
2) Chirp Configuration (unique for each AWR device - mainly because TXs to use are
different for each chirp)
3) Frame Configuration (common to all 4 AWR devices, except for the trigger mode for the master)
Change the values below as needed. --]]
-- Profile configuration
local profile_indx = 0
local start_freq = 76.284 -- GHz
local slope = 3.911 -- MHz/us
local idle_time = 5 -- us
local adc_start_time = 4 -- us
local adc_samples = 1024 -- Number of samples per chirp
local sample_freq = 10000 -- ksps
local ramp_end_time = 110.4 -- us
local rx_gain = 48 -- dB
local tx0OutPowerBackoffCode = 0
local tx1OutPowerBackoffCode = 0
local tx2OutPowerBackoffCode = 0
local tx0PhaseShifter = 0
local tx1PhaseShifter = 0
local tx2PhaseShifter = 0
local txStartTimeUSec = 0
local hpfCornerFreq1 = 0 -- 0: 175KHz, 1: 235KHz, 2: 350KHz, 3: 700KHz
local hpfCornerFreq2 = 0 -- 0: 350KHz, 1: 700KHz, 2: 1.4MHz, 3: 2.8MHz
-- Frame configuration
local start_chirp_tx = 0
local end_chirp_tx = 3
local nchirp_loops = 64 -- Number of chirps per frame
local nframes_master = 10 -- Number of Frames for Master
local Inter_Frame_Interval = 100 -- ms
local trigger_delay = 0 -- us
local trig_list = {1,2,2,2} -- 1: Software trigger, 2: Hardware trigger
--[[
Function to configure the chirps specific to a device
12 chirps are configured below, individually for each AWR device
|-------|-------|-------|-------|-------|-------|-------|-------|-------|-------|-------|-------|-------|
| | Dev 1 | Dev 1 | Dev 1 | Dev 2 | Dev 2 | Dev 2 | Dev 3 | Dev 3 | Dev 3 | Dev 4 | Dev 4 | Dev 4 |
| Chirp | TX0 | TX1 | TX2 | TX 0 | TX1 | TX2 | TX0 | TX1 | TX2 | TX0 | TX1 | TX2 |
|-------|-------|-------|-------|-------|-------|-------|-------|-------|-------|-------|-------|-------|
| 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 |
| 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 |
| 2 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 |
| 3 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 |
| 4 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 |
| 5 | 0 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 |
| 6 | 0 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 |
| 7 | 0 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| 8 | 0 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| 9 | 0 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| 10 | 0 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
| 11 | 1 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 | 0 |
|-------|-------|-------|-------|-------|-------|-------|-------|-------|-------|-------|-------|-------|
--]]
-- Note: The syntax for this API is:
-- ar1.ChirpConfig_mult(RadarDeviceId, chirpStartIdx, chirpEndIdx, profileId, startFreqVar,
-- freqSlopeVar, idleTimeVar, adcStartTimeVar, tx0Enable, tx1Enable, tx2Enable)
function Configure_Chirps(i)
if (i == 1) then
-- Chirp 0
if (0 == ar1.ChirpConfig_mult(dev_list[i], 0, 0, 0, 0, 0, 0, 0, 1, 0, 0)) then
WriteToLog("Device "..i.." : Chirp 0 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 0 Configuration failed\n", "red")
return -4
end
-- Chirp 1
if (0 == ar1.ChirpConfig_mult(dev_list[i], 1, 1, 0, 0, 0, 40, 0, 1, 0, 0)) then
WriteToLog("Device "..i.." : Chirp 1 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 1 Configuration failed\n", "red")
return -4
end
-- Chirp 2
if (0 == ar1.ChirpConfig_mult(dev_list[i], 2, 2, 0, 0, 0, 14, 0, 1, 0, 0)) then
WriteToLog("Device "..i.." : Chirp 2 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 2 Configuration failed\n", "red")
return -4
end
-- Chirp 3
if (0 == ar1.ChirpConfig_mult(dev_list[i], 3, 3, 0, 0, 0, 14, 0, 0, 1, 0)) then
WriteToLog("Device "..i.." : Chirp 3 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 3 Configuration failed\n", "red")
return -4
end
elseif (i == 2) then
-- Chirp 0
if (0 == ar1.ChirpConfig_mult(dev_list[i], 0, 0, 0, 0, 0, 0, 0, 1, 0, 0)) then
WriteToLog("Device "..i.." : Chirp 0 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 0 Configuration failed\n", "red")
return -4
end
-- Chirp 1
if (0 == ar1.ChirpConfig_mult(dev_list[i], 1, 1, 0, 0, 0, 40, 0, 1, 0, 0)) then
WriteToLog("Device "..i.." : Chirp 1 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 1 Configuration failed\n", "red")
return -4
end
-- Chirp 2
if (0 == ar1.ChirpConfig_mult(dev_list[i], 2, 2, 0, 0, 0, 14, 0, 1, 0, 0)) then
WriteToLog("Device "..i.." : Chirp 2 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 2 Configuration failed\n", "red")
return -4
end
-- Chirp 3
if (0 == ar1.ChirpConfig_mult(dev_list[i], 3, 3, 0, 0, 0, 14, 0, 0, 1, 0)) then
WriteToLog("Device "..i.." : Chirp 3 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 3 Configuration failed\n", "red")
return -4
end
elseif (i == 3) then
-- Chirp 0
if (0 == ar1.ChirpConfig_mult(dev_list[i], 0, 0, 0, 0, 0, 0, 0, 1, 0, 0)) then
WriteToLog("Device "..i.." : Chirp 0 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 0 Configuration failed\n", "red")
return -4
end
-- Chirp 1
if (0 == ar1.ChirpConfig_mult(dev_list[i], 1, 1, 0, 0, 0, 40, 0, 1, 0, 0)) then
WriteToLog("Device "..i.." : Chirp 1 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 1 Configuration failed\n", "red")
return -4
end
-- Chirp 2
if (0 == ar1.ChirpConfig_mult(dev_list[i], 2, 2, 0, 0, 0, 14, 0, 1, 0, 0)) then
WriteToLog("Device "..i.." : Chirp 2 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 2 Configuration failed\n", "red")
return -4
end
-- Chirp 3
if (0 == ar1.ChirpConfig_mult(dev_list[i], 3, 3, 0, 0, 0, 14, 0, 0, 1, 0)) then
WriteToLog("Device "..i.." : Chirp 3 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 3 Configuration failed\n", "red")
return -4
end
elseif (i == 4) then
-- Chirp 0
if (0 == ar1.ChirpConfig_mult(dev_list[i], 0, 0, 0, 0, 0, 0, 0, 1, 0, 0)) then
WriteToLog("Device "..i.." : Chirp 0 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 0 Configuration failed\n", "red")
return -4
end
-- Chirp 1
if (0 == ar1.ChirpConfig_mult(dev_list[i], 1, 1, 0, 0, 0, 40, 0, 1, 0, 0)) then
WriteToLog("Device "..i.." : Chirp 1 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 1 Configuration failed\n", "red")
return -4
end
-- Chirp 2
if (0 == ar1.ChirpConfig_mult(dev_list[i], 2, 2, 0, 0, 0, 14, 0, 1, 0, 0)) then
WriteToLog("Device "..i.." : Chirp 2 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 2 Configuration failed\n", "red")
return -4
end
-- Chirp 3
if (0 == ar1.ChirpConfig_mult(dev_list[i], 3, 3, 0, 0, 0, 14, 0, 0, 1, 0)) then
WriteToLog("Device "..i.." : Chirp 3 Configuration successful\n", "green")
else
WriteToLog("Device "..i.." : Chirp 3 Configuration failed\n", "red")
return -4
end
end
end
------------------------------ API Configuration ------------------------------------------------
-- 1. Connection to TDA. 2. Selecting Cascade/Single Chip. 3. Selecting 2-chip/4-chip
WriteToLog("Setting up Studio for Cascade started..\n", "blue")
if(0 == ar1.ConnectTDA(TDA_IPAddress, 5001, deviceMapOverall)) then
WriteToLog("ConnectTDA Successful\n", "green")
else
WriteToLog("ConnectTDA Failed\n", "red")
return -1
end
if(0 == ar1.selectCascadeMode(1)) then
WriteToLog("selectCascadeMode Successful\n", "green")
else
WriteToLog("selectCascadeMode Failed\n", "red")
return -1
end
WriteToLog("Setting up Studio for Cascade ended..\n", "blue")
--Master Initialization
-- SOP Mode Configuration
if (0 == ar1.SOPControl_mult(1, 4)) then
WriteToLog("Master : SOP Reset Successful\n", "green")
else
WriteToLog("Master : SOP Reset Failed\n", "red")
return -1
end
-- SPI Connect
if (0 == ar1.PowerOn_mult(1, 0, 1000, 0, 0)) then
WriteToLog("Master : SPI Connection Successful\n", "green")
else
WriteToLog("Master : SPI Connection Failed\n", "red")
return -1
end
-- Firmware Download. (SOP 4 - MetaImage)
if (0 == ar1.DownloadBssFwOvSPI_mult(1, metaImagePath)) then
WriteToLog("Master : FW Download Successful\n", "green")
else
WriteToLog("Master : FW Download Failed\n", "red")
return -1
end
-- RF Power Up
if (0 == ar1.RfEnable_mult(1)) then
WriteToLog("Master : RF Power Up Successful\n", "green")
else
WriteToLog("Master : RF Power Up Failed\n", "red")
return -1
end
-- Channel & ADC Configuration
if (0 == ar1.ChanNAdcConfig_mult(1,1,1,1,1,1,1,1,2,1,0,1)) then
WriteToLog("Master : Channel & ADC Configuration Successful\n", "green")
else
WriteToLog("Master : Channel & ADC Configuration Failed\n", "red")
return -2
end
-- All devices together
-- Including this depends on the type of board being used.
-- LDO configuration
if (0 == ar1.RfLdoBypassConfig_mult(deviceMapOverall, 3)) then
WriteToLog("LDO Bypass Successful\n", "green")
else
WriteToLog("LDO Bypass failed\n", "red")
return -2
end
-- Low Power Mode Configuration
if (0 == ar1.LPModConfig_mult(deviceMapOverall,0, 0)) then
WriteToLog("Low Power Mode Configuration Successful\n", "green")
else
WriteToLog("Low Power Mode Configuration failed\n", "red")
return -2
end
-- Miscellaneous Control Configuration
if (0 == ar1.SetMiscConfig_mult(deviceMapOverall, 1, 0, 0, 0)) then
WriteToLog("Misc Control Configuration Successful\n", "green")
else
WriteToLog("Misc Control Configuration failed\n", "red")
return -2
end
-- Edit this API to enable/disable the boot time calibration. Enabled by default.
-- RF Init Calibration Configuration
if (0 == ar1.RfInitCalibConfig_mult(deviceMapOverall, 1, 1, 1, 1, 1, 1, 1, 65537)) then
WriteToLog("RF Init Calibration Successful\n", "green")
else
WriteToLog("RF Init Calibration failed\n", "red")
return -2
end
-- RF Init
if (0 == ar1.RfInit_mult(deviceMapOverall)) then
WriteToLog("RF Init Successful\n", "green")
else
WriteToLog("RF Init failed\n", "red")
return -2
end
---------------------------Data Configuration----------------------------------
-- Data path Configuration
if (0 == ar1.DataPathConfig_mult(deviceMapOverall, 0, 1, 0)) then
WriteToLog("Data Path Configuration Successful\n", "green")
else
WriteToLog("Data Path Configuration failed\n", "red")
return -3
end
-- Clock Configuration
if (0 == ar1.LvdsClkConfig_mult(deviceMapOverall, 1, 1)) then
WriteToLog("Clock Configuration Successful\n", "green")
else
WriteToLog("Clock Configuration failed\n", "red")
return -3
end
-- CSI2 Configuration
if (0 == ar1.CSI2LaneConfig_mult(deviceMapOverall, 1, 0, 2, 0, 4, 0, 5, 0, 3, 0, 0)) then
WriteToLog("CSI2 Configuration Successful\n", "green")
else
WriteToLog("CSI2 Configuration failed\n", "red")
return -3
end
----------------------------Test Source Configuration------------------------------
-- This is useful for initial bringup.
-- Each device is configured with a test object at a different location.
if(test_source_enable == 1) then
if(RadarDevice[1] == 1) then
-- Object at 5 m with x = 4m and y = 3m
if (0 == ar1.SetTestSource_mult(1, 4, 3, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0,
0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0, 0)) then
WriteToLog("Device 1 : Test Source Configuration Successful\n", "green")
else
WriteToLog("Device 1 : Test Source Configuration failed\n", "red")
return -3
end
end
if(RadarDevice[2] == 1) then
-- Object at 5 m with x = 3m and y = 4m
if (0 == ar1.SetTestSource_mult(2, 3, 4, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0,
0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0, 0)) then
WriteToLog("Device 2 : Test Source Configuration Successful\n", "green")
else
WriteToLog("Device 2 : Test Source Configuration failed\n", "red")
return -3
end
end
if(RadarDevice[3] == 1) then
-- Object at 13 m with x = 12m and y = 5m
if (0 == ar1.SetTestSource_mult(4, 12, 5, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0,
0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0, 0)) then
WriteToLog("Device 3 : Test Source Configuration Successful\n", "green")
else
WriteToLog("Device 3 : Test Source Configuration failed\n", "red")
return -3
end
end
if(RadarDevice[4] == 1) then
-- Object at 13 m with x = 5m and y = 12m
if (0 == ar1.SetTestSource_mult(8, 5, 12, 0, 0, 0, 0, -327, 0, -327, 327, 327, 327, -2.5, 327, 327, 0,
0, 0, 0, -327, 0, -327, 327, 327, 327, -95, 0, 0, 0.5, 0, 1, 0, 1.5, 0, 0, 0, 0, 0, 0, 0, 0)) then
WriteToLog("Device 4 : Test Source Configuration Successful\n", "green")
else
WriteToLog("Device 4 : Test Source Configuration failed\n", "red")
return -3
end
end
end
---------------------------Sensor Configuration-------------------------
-- Profile Configuration
if (0 == ar1.ProfileConfig_mult(deviceMapOverall, 0, start_freq, idle_time, adc_start_time, ramp_end_time,
0, 0, 0, 0, 0, 0, slope, 0, adc_samples, sample_freq, 0, 0, rx_gain)) then
WriteToLog("Profile Configuration successful\n", "green")
else
WriteToLog("Profile Configuration failed\n", "red")
return -4
end
-- Chirp Configuration
for i=1,table.getn(RadarDevice) do
if ((RadarDevice[1]==1) and (RadarDevice[i]==1)) then
Configure_Chirps(i)
end
end
-- Enabling/ Disabling Test Source
if(test_source_enable == 1) then
ar1.EnableTestSource_mult(deviceMapOverall, 1)
WriteToLog("Enabling Test Source Configuration successful\n", "green")
end
-- Frame Configuration
-- Master
if (0 == ar1.FrameConfig_mult(1,start_chirp_tx,end_chirp_tx,nframes_master, nchirp_loops,
Inter_Frame_Interval, 0, 1)) then
WriteToLog("Master : Frame Configuration successful\n", "green")
else
WriteToLog("Master : Frame Configuration failed\n", "red")
end
在使用cascade_capture_contstream.lua的时候,有时报错,然后软件重启就好了,但是收发的信号用仪器检测出来的确是单载波,代码如下:
--[[
A. STREAMING & CAPTURE
1. Streaming Slave (3, 2, 1) sequentially.
2. Streaming Master.
B. TRANSFERRING FILES
1. The data is stored in file(s) with max cap placed at 2 GB.
2. The files can be retrieved from the SSD (/mnt/ssd folder) using WinSCP.
Note: Update lines 18 to 66 as needed before using this script.
--]]
--------------------------- Streaming Configuration -------------------------------------------
-- Change the values below as needed.
-- Streaming configuration
local start_freq = 76.284 -- GHz
local sample_freq = 10000 -- ksps
local rx_gain = 48 -- dB
local tx0OutPowerBackoffCode = 0
local tx1OutPowerBackoffCode = 0
local tx2OutPowerBackoffCode = 0
local tx0PhaseShifter = 0
local tx1PhaseShifter = 0
local tx2PhaseShifter = 0
local hpfCornerFreq1 = 0 -- 0: 175KHz, 1: 235KHz, 2: 350KHz, 3: 700KHz
local hpfCornerFreq2 = 0 -- 0: 350KHz, 1: 700KHz, 2: 1.4MHz, 3: 2.8MHz
-- Basic configuration for Analysis
local numSamples = 524288
-- Streaming Configuration
if (0 == ar1.ContStrConfig_mult(deviceMapOverall, start_freq, sample_freq, rx_gain, hpfCornerFreq1,
hpfCornerFreq2, tx0OutPowerBackoffCode, tx1OutPowerBackoffCode, tx2OutPowerBackoffCode,
tx0PhaseShifter, tx1PhaseShifter, tx2PhaseShifter)) then
WriteToLog("Streaming Configuration successful\n", "green")
else
WriteToLog("Streaming Configuration failed\n", "red")
return -4
end
-- Note: "capture_time" is a timeout till which the devices are streaming continuously.
-- It does not affect the amount of data/samples being captured by the TDA2XX.
-- Data captured by TDA2XX depends on the number of samples being programmed at line 31
capture_time = 20000 -- ms
inter_loop_time = 2000 -- ms
num_loops = 1
--[[
Note:
Change the parameter as desired:
1. capture_directory: is the filename under which captures are stored on the SSD
and is also the directory to which files will be transferred back to the host
The captures are copied to the PostProc folder within mmWave Studio.
Note:
If this script is called multiple times without changing the directory name, then all
captured files will be in the same directory with filename suffixes incremented automatically.
It may be hard to know which captured files correspond to which run of the script.
Note:
It is strongly recommended to change this directory name between captures.
--]]
------------------------------DATA CAPTURE------------------------------
-- Function to start/stop Streaming
function Streaming_Control(Device_ID, En1_Dis0)
local status = 0
if (En1_Dis0 == 1) then
status = ar1.ContStrModEnable_mult(dev_list[Device_ID]) --Start Streaming
if (status == 0) then
WriteToLog("Device "..Device_ID.." : Start Streaming Successful\n", "green")
else
WriteToLog("Device "..Device_ID.." : Start Streaming Failed\n", "red")
return -5
end
else
status = ar1.ContStrModDisable_mult(dev_list[Device_ID]) --Stop Streaming
if (status == 0) then
WriteToLog("Device "..Device_ID.." : Stop Streaming Successful\n", "green")
else
WriteToLog("Device "..Device_ID.." : Stop Streaming Failed\n", "red")
return -5
end
end
return status
end
while (num_loops > 0)
do
WriteToLog("Loops Remaining : "..num_loops.."\n", "purple")
-- Start Streaming
WriteToLog("Starting Streaming Start sequence...\n", "blue")
if (RadarDevice[4]==1)then
Streaming_Control(4,1)
end
if (RadarDevice[3]==1)then
Streaming_Control(3,1)
end
if (RadarDevice[2]==1)then
Streaming_Control(2,1)
end
Streaming_Control(1,1)
RSTD.Sleep(1000)
-- Basic Configuration for Analysis
if (0 == ar1.BasicConfigurationForAnalysis(numSamples, numSamples, 1, 0, 0, 0, 1)) then
WriteToLog("Basic Configuration for Analysis successful\n", "green")
else
WriteToLog("Basic Configuration for Analysis failed\n", "red")
return -4
end
RSTD.Sleep(1000)
-- TDA ARM
capture_directory = "Cascade_22xx_Cont_Stream_Capture_"..num_loops.."_iteration"
WriteToLog("Starting TDA ARM for Cont Stream...\n", "blue")
status = ar1.TDAContStream_StartRecord_mult(1, capture_directory)
if (status == 0) then
WriteToLog("TDA ARM for Cont Stream Successful\n", "green")
else
WriteToLog("TDA ARM for Cont Stream Failed\n", "red")
return -5
end
WriteToLog("Capturing AWR device data to the TDA SSD...\n", "blue")
RSTD.Sleep(capture_time)
-- Stop Streaming
WriteToLog("Starting Streaming Stop sequence...\n", "blue")
if (RadarDevice[4]==1)then
Streaming_Control(4,0)
end
if (RadarDevice[3]==1)then
Streaming_Control(3,0)
end
if (RadarDevice[2]==1)then
Streaming_Control(2,0)
end
Streaming_Control(1,0)
WriteToLog("Capture sequence completed...\n", "blue")
num_loops = num_loops - 1
RSTD.Sleep(inter_loop_time)
end
-- Enable the below if required
WriteToLog("Starting Transfer files using WinSCP for Cont Stream..\n", "blue")
status = ar1.TransferFilesUsingWinSCPContStream_mult(1)
if(status == 0) then
WriteToLog("Transferred files! COMPLETE!\n", "green")
else
WriteToLog("Transferring files FAILED!\n", "red")
return -5
end
请问
1.这个脚本是只能发射单载波吗,不是发射连续波的脚本吗?
2.我上面配置好的连续波,应该如何收发呢,可以在mmwave studio上面直接点相应的发射和接受按键吗,是哪些按键呢?
3.如果通过脚本实现收发,应该怎么操作呢?