This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2212: 咨询FDC2212的精度和速度相关问题

Part Number: FDC2212
Other Parts Discussed in Thread: FDC2214

您好:

         我想问一下芯片FDC2212或者FDC2214,我看手册中写的均方根噪声是0.3fF,测试条件是在100sps且传感器频率为5M时,我想问一下这个0.3fF是如何计算出来的?因为我依据手册里面的转换频率,有效位数等算出来的精度比这个大很多。

       目前,我想在项目中做高精度电容解算用于微位移测量。我要测的电容容值范围是1pF到30pF,需要测的最小电容为0.00145pF,需要的采样率为1ms(1k),我想核一下咱们这款芯片可以满足这样的需求吗?

    期待您的回复,万分感谢!