工程师你好,
最近在使用AWR2944EVM,使用EVM的OOB中的enetStream demo时遇到了如下问题。希望可以帮忙解答,非常感谢
1.在使用visualizer发送。cfg文件时,可以正常配置以太网,并可以从tcpserver.py中读取到数据。
2.通过CLI_ByPassApi()函数配置以太网参数时,会出现问题,如图1所示,在配置完以太网的remoteIp之后,板子就无响应了,(图中表示为done只打印了don),

图1
图2为radarcmdString中的配置信息

图2
3.我确认localIP已经被正确配置,连接方式为EVM-router-PC,router具有DHCP功能,通过queryLocalIP得到LocalIP的地址为172.168.4.207,remoteIp为172.168.4.195
#ifndef CLI_BYPASS
#define CLI_BYPASS
static void CLI_task(void* args)
{
#ifndef CLI_BYPASS
uint8_t cmdString[READ_LINE_BUFSIZE];
char* tokenizedArgs[CLI_MAX_ARGS];
char* ptrCLICommand;
char delimitter[] = " \r\n";
uint32_t argIndex;
CLI_CmdTableEntry* ptrCLICommandEntry;
int32_t cliStatus, status;
uint32_t index;
/* Do we have a banner to be displayed? */
if (gCLI.cfg.cliBanner != NULL)
{
/* YES: Display the banner */
CLI_write (gCLI.cfg.cliBanner);
}
CLI_write("CLI_task\n");
while(1)
{
if(enet_init_flag)
{
CLI_write("get localIp\n");
break;
}
}
/* Loop around forever: */
while (1)
{
/* Demo Prompt: */
CLI_write (gCLI.cfg.cliPrompt);
/* Reset the command string: */
memset ((void *)&cmdString[0], 0, sizeof(cmdString));
status = CLI_readLine(gCLI.cfg.cliUartHandle, (char*)&cmdString[0], READ_LINE_BUFSIZE);
if(status != SystemP_SUCCESS)
{
CLI_write("Error reading\n");
}
/* Reset all the tokenized arguments: */
memset ((void *)&tokenizedArgs, 0, sizeof(tokenizedArgs));
argIndex = 0;
ptrCLICommand = (char*)&cmdString[0];
/* comment lines found - ignore the whole line*/
if (cmdString[0]=='%' || cmdString[1]=='%')
{
CLI_write ("Skipped\n");
continue;
}
/* Set the CLI status: */
cliStatus = -1;
/* The command has been entered we now tokenize the command message */
while (1)
{
/* Tokenize the arguments: */
tokenizedArgs[argIndex] = strtok(ptrCLICommand, delimitter);
if (tokenizedArgs[argIndex] == NULL)
break;
/* Increment the argument index: */
argIndex++;
if (argIndex >= CLI_MAX_ARGS)
break;
/* Reset the command string */
ptrCLICommand = NULL;
}
/* Were we able to tokenize the CLI command? */
if (argIndex == 0)
continue;
/* Cycle through all the registered CLI commands: */
for (index = 0; index < gCLI.numCLICommands; index++)
{
ptrCLICommandEntry = &gCLI.cfg.tableEntry[index];
/* Do we have a match? */
if (strcmp(ptrCLICommandEntry->cmd, tokenizedArgs[0]) == 0)
{
/* YES: Pass this to the CLI registered function */
cliStatus = ptrCLICommandEntry->cmdHandlerFxn (argIndex, tokenizedArgs);
if (cliStatus == 0)
{
CLI_write ("Done\r\n");
}
else
{
CLI_write ("Error %d\r\n", cliStatus);
}
break;
}
}
/* Did we get a matching CLI command? */
if (index == gCLI.numCLICommands)
{
/* NO matching command found. Is the mmWave extension enabled? */
if (gCLI.cfg.enableMMWaveExtension == 1U)
{
/* Yes: Pass this to the mmWave extension handler */
cliStatus = CLI_MMWaveExtensionHandler (argIndex, tokenizedArgs);
}
/* Was the CLI command found? */
if (cliStatus == -1)
{
/* No: The command was still not found */
CLI_write ("'%s' is not recognized as a CLI command\n", tokenizedArgs[0]);
}
}
}
#else
CLI_write("BYPASS_API\n");
if(enet_init_flag)
CLI_write("LocalIp have been set\n");
CLI_ByPassApi(&gCLI.cfg);
CLI_write("LocalIp SET\n");
#endif
}
#endif