This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: 如何确定天线发送顺序?

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1843

你好,

        在chirp配置中有个txEnable,可以使能需要发送的天线位,

/**
* @brief Tx enable selection bit mask \n
b0 Enable TX0 \n
0 Tx0 Disable \n
1 Tx0 Enable \n
b1 Enable TX1 \n
0 Tx1 Disable \n
1 Tx1 Enable \n
b2 Enable TX2 \n
0 Tx2 Disable \n
1 Tx2 Enable \n
@note : Maximum of only 2 TX can be turned in a chirp \n
*/

注释是这样解释的,可以最多配置两个位,假设配置成3,也就是Tx0 Enable   1 Tx1 Enable 0 Tx2 Disable

那在实际发射中是怎样处理的,是每个chirp中,TX0 和TX1 交替发射,还是第一个chirp发射TX0,第二个chirp发射TX1