Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1843
你好,
在chirp配置中有个txEnable,可以使能需要发送的天线位,
/**
* @brief Tx enable selection bit mask \n
b0 Enable TX0 \n
0 Tx0 Disable \n
1 Tx0 Enable \n
b1 Enable TX1 \n
0 Tx1 Disable \n
1 Tx1 Enable \n
b2 Enable TX2 \n
0 Tx2 Disable \n
1 Tx2 Enable \n
@note : Maximum of only 2 TX can be turned in a chirp \n
*/
注释是这样解释的,可以最多配置两个位,假设配置成3,也就是Tx0 Enable 1 Tx1 Enable 0 Tx2 Disable
那在实际发射中是怎样处理的,是每个chirp中,TX0 和TX1 交替发射,还是第一个chirp发射TX0,第二个chirp发射TX1