This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMCS1100: 供电电压选择

Part Number: TMCS1100


这款传感器是可以双向采样电流的,想问下能否这样供电 

Vs接+5V

Vref接地

GND引脚接-5V

这样输出的采样信号是否可以在±5V之间变化,反映电流的双向?

使用情况:采样双向变化的±10A电流,希望传感器输出的信号没有直流偏置,也就是0A时输出0V