您好,我想请问一下ADCBUFF里面存放4根接收天线的顺序是否为上半部分为奇数,下半部分为偶数天线的数据,而不是给出的下图所示文档中的这样的排列顺序。
用于 XWR16XX 的毫米波 (mmw) 演示

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我想请问一下ADCBUFF里面存放4根接收天线的顺序是否为上半部分为奇数,下半部分为偶数天线的数据,而不是给出的下图所示文档中的这样的排列顺序。
用于 XWR16XX 的毫米波 (mmw) 演示

你好,
请问你看的是mmwave sdk3.5的代码么?
图上的数据存放是按接收天线R1,RX2,RX3,Rx4,并不是你说的上半部分为奇数天线,下半部分为偶数天线。
在mmw demo里面根据下面的代码可知,接收到一个chirp所有接收天线的数据就会产生chirp中断,进行数据搬移。而上图是接收到2个chrip的所有接收天线的示例,和mmw demo在这点上是有区别的。
ADCBuf_Handle MmwDemo_ADCBufOpen(SOC_Handle socHandle)
{。。。
ADCBufparams.chirpThresholdPing = 1;
ADCBufparams.chirpThresholdPong = 1;
Adcbuf_mmwave.c (packages\ti\drivers\adcbuf\src): ADCBUFSetPingNumChirpThreshhold(ptrDssRegBase, ((uint32_t)params->chirpThresholdPing - 1U));
您好,我使用的是SDK2.0,这个是他给的docs里面的存放数据的格式,它是按照R1,R2,R3,R4的顺序吗。这里放置的chirp数是否由
这个变量决定。