This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: The board reported an error.

Part Number: AWR1843BOOST


1、Probability error occurs during power-on. Indicator DS1 is red on (hardware error occurs)

2、When the configuration program is loaded through the upper computer, the indicator DS1 is red on

 

In a word, the board is unstable and the error rate is very high. Please confirm whether it can be returned and replaced. Thank you!

It has been confirmed that there is no problem with the power supply, or the error is still reported. Because there is a problem with the new one, the seller asked us to find TI's engineer to confirm the quality problem and contact Mouser to return and replace the goods. thank you

  • 请按照以下方式联系客户支持部门的技术部门,会有技术客服为您提供帮助。

    • 打开链接https://ticsc.service-now.com/csm
    • 点击申请新的支持下面的提交申请按钮
    • 在新打开的窗口中点击技术支持下面的创建案例按钮
    • 在打开的表格中您可以使用中文描述您的问题并且递交。递交申请时,请您提及以下信息:
      • Ti.com购买订单号
      • 需要技术鉴定EVM是否存在质量问题
      • 您是否使用免费邮箱注册myti账号