Other Parts Discussed in Thread: UNIFLASH
尊敬的TI工程师你好,我用AWR1642BOOST 测试driver vital signs 的时候前一天还是正常的,第二天测试时上位机GUI就不显示图形了,结果如下:
QT version = 5.9.1 QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted() Serial Port Found Data Port Number is "COM5" User Port Number is "COM4" Data port succesfully Open User port succesfully Open Configuration File Name Read from the GUI is %s/n "xwr1642_profile_VitalSigns_20fps_Back.cfg" QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted() "COM4" Configuration File Path is %s/n "D:/tools/labs/lab0001-driver-vital-signs/vitalSigns_host/profiles/xwr1642_profile_VitalSigns_20fps_Front.cfg" "sensorStop" "flushCfg" "dfeDataOutputMode 1" "channelCfg 15 3 0" "adcCfg 2 1" "adcbufCfg -1 0 0 1 0" "profileCfg 0 77 7 6 57 0 0 70 1 200 4000 0 0 48" "chirpCfg 0 0 0 0 0 0 0 1" "frameCfg 0 0 2 0 50 1 0" "lowPower 0 1" "guiMonitor 0 0 0 0 1" "calibDcRangeSig -1 0 0 0 0" "vitalSignsCfg 0.3 0.9 256 512 4 0.1 0.05 100000 300000" "motionDetection 1 20 2.0 0" "sensorStart" ""
我尝试用UniFlash重新烧录下位机程序的时候,出现错误,结果如下:
[2022/9/19 上午10:59:04] [INFO] Cortex_R4_0: Reset connection to device
[2022/9/19 上午10:59:04] [INFO] Cortex_R4_0: Set break signal
[2022/9/19 上午10:59:24] [ERROR] Cortex_R4_0: Initial response from the device was not received. Please power cycle device before re-flashing.
[2022/9/19 上午10:59:24] [ERROR] Cortex_R4_0: Not able to connect to serial port. Recheck COM port selected and/or permissions.
[2022/9/19 上午10:59:24] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...
请问这个要怎么解决