This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: 下位机无法接收上位机发送的串口指令

Part Number: AWR1642BOOST
Other Parts Discussed in Thread: UNIFLASH

尊敬的TI工程师你好,我用AWR1642BOOST 测试driver vital signs 的时候前一天还是正常的,第二天测试时上位机GUI就不显示图形了,结果如下:

QT version =  5.9.1
QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted()
Serial Port Found
Data Port Number is "COM5"
User Port Number is "COM4"
Data port succesfully Open
User port succesfully Open
Configuration File Name Read from the GUI is %s/n "xwr1642_profile_VitalSigns_20fps_Back.cfg"
QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted()
"COM4"
Configuration File Path is %s/n "D:/tools/labs/lab0001-driver-vital-signs/vitalSigns_host/profiles/xwr1642_profile_VitalSigns_20fps_Front.cfg"
"sensorStop"
"flushCfg"
"dfeDataOutputMode 1"
"channelCfg 15 3 0"
"adcCfg 2 1"
"adcbufCfg -1 0 0 1 0"
"profileCfg 0 77 7 6 57 0 0 70 1 200 4000 0 0 48"
"chirpCfg 0 0 0 0 0 0 0 1"
"frameCfg 0 0 2 0 50 1 0"
"lowPower 0 1"
"guiMonitor 0 0 0 0 1"
"calibDcRangeSig -1 0 0 0 0"
"vitalSignsCfg 0.3 0.9 256 512 4 0.1 0.05 100000 300000"
"motionDetection 1 20 2.0 0"
"sensorStart"
""

我尝试用UniFlash重新烧录下位机程序的时候,出现错误,结果如下:

[2022/9/19 上午10:59:04] [INFO] Cortex_R4_0: Reset connection to device
[2022/9/19 上午10:59:04] [INFO] Cortex_R4_0: Set break signal
[2022/9/19 上午10:59:24] [ERROR] Cortex_R4_0: Initial response from the device was not received. Please power cycle device before re-flashing.
[2022/9/19 上午10:59:24] [ERROR] Cortex_R4_0: Not able to connect to serial port. Recheck COM port selected and/or permissions.
[2022/9/19 上午10:59:24] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...

请问这个要怎么解决