电路采用单端模式,电感18uH,电容33pF,手册中推荐电路
如下图,单端模式使用外部输入频率应小于35MHz,外部时钟选择40MHz,时钟分频是否必须是2分频?

如下图,根据电容电感和PCB寄生电容,计算传感器频率为5.15MHz,外部分频后输入时钟Fref大于4倍5.15MHz,外部输入时钟应大于20MHz,不能分频,与上述必须小于35Mhz是否冲突?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电路采用单端模式,电感18uH,电容33pF,手册中推荐电路
如下图,单端模式使用外部输入频率应小于35MHz,外部时钟选择40MHz,时钟分频是否必须是2分频?

如下图,根据电容电感和PCB寄生电容,计算传感器频率为5.15MHz,外部分频后输入时钟Fref大于4倍5.15MHz,外部输入时钟应大于20MHz,不能分频,与上述必须小于35Mhz是否冲突?

您好,第一个问题和e2echina.ti.com/.../fdc2212-fdc2212
重复了,可以参考上述链接哈。
第二个问题, fREF0 is > 4 × fSENSOR,fsensor频率为5.15MHz,那么fref0需要大于20.6Mhz。
而fREF0=fCLK/ CH0_FREF_DIVIDER.
fCLK即为外部输入时钟。 因此fclk<35Mhz,而fREF0需要大于20.6Mhz,那么 CH0_FREF_DIVIDER只能为1.
即您附上的上述介绍中说的:reference divider should be 1.