This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2212: FDC2212单端模式,时钟输入应该是多少

Part Number: FDC2212


单端模式,外部输入40MHz,Fref理应小于35MHz,是否必须两分频?

  • 您好,FDC2212的输入时钟可以使用内部有源晶振提供,也可以是外部时钟输入CLKIN作为参考时钟。

    单端模式下,参考Table1,输入时钟频率Fref要小于35Mhz。

    并且单端模式下,CHx_FIN_SEL  bit需要配置为10,即二分频。

  • CHx_FIN_SEL  bit不是设置传感器频率分频的吗?

    CH0_FREF_DIVIDER (0x14)是设置外部输入时钟分频

  • 您好,您的理解是对的,CHx_FIN_SEL是传感器频率的分频。传感器单端模式下,CHx_FIN_SEL  bit需要二分频,配置为10.

    参考下图比较直观。

    您的问题是如果外部时钟输入40Mhz,CH0_FREF_DIVIDER 分频系数n是否需要2分频是吗?

    假设2分频的话,则fREFx=20Mhz,而单端模式下受到 fREF0 is > 4 × fSENSOR的限制,如果fsensor频率为5.15MHz,那么fref0需要大于20.6Mhz。

    所以n=2的话,虽然满足fREF小于35Mhz的条件,但是不满足 fREF0 is > 4 × fSENSOR的限制。

    那么我们可以更改输入时钟频率CLKIN,CLKIN的频率范围为2~40Mhz。