This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我在使用Programmer Standalone 3.12 SP1 64-bit for Windows(不是PDF上列出的3.10版本)刷新DCA1000EVM中的FPGA bit(DCA1000_FPGA_RECORD_V2.8_05JUL2019.bit)文件时遇到以下问题:
我按要求下载了Diamond Programmer,并按照PDF上的步骤进行刷新,到达以下这一步时要求Device和Package,但我从器件下拉菜单中并没有找到PDF上列出的Device: SPI-N25Q128A与Package: 16-pin SO16。如何解决?
谢谢!
请看一下S1是否按照Figure 20. FPGA Config Switch配置的?
https://www.ti.com.cn/cn/lit/ug/spruij4a/spruij4a.pdf
另外,板子和PC是通过网线直接相连的吗?防火墙和杀毒软件都关了吧。
如果上面都没问题的话,建议咨询一下lattice公司是不是Diamond programmer软件本身的问题。