Other Parts Discussed in Thread: UNIFLASH, IWR6843
您好:
我在使用uniflsh7.1.0烧录IWR6843ISK时,点击load image后一直卡在这个界面

我确定所使用的接口是正确的,所烧录文件的路径没有中文,并且更换PC后没有得到解决
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请对照下面的培训视频看一下板子的配置和烧写步骤,看是否一样的操作?
https://training.ti.com/hardware-setup-iwr6843isk-and-iwr6843isk-ods
我这边烧写了一下,没有问题。
您看一下在uniflash里device是否选择了IWR6843ISK? 另外,电脑的杀毒软件,防火墙是否都关了?会用到串口的软件如ccs等是否也关了?
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: Initialization complete.
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: Flashing process starting...
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: Connecting to COM Port COM19...
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: Reset connection to device
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: Set break signal
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: Connection to COM port succeeded. Flashing can proceed.
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: Reading device version info...
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: ** 1 files specified for flashing.
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: Checking file C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr68xx/mmw/xwr68xx_mmw_demo.bin for correct header for IWR6843.
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: IWR6843 device, fileType=META_IMAGE1 detected -> OK
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: !! Files are valid for IWR6843.
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: Format on download was specified. Formatting SFLASH storage...
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: -->Erasing storage [SFLASH]
[11/2/2022, 10:21:02 AM] [INFO] Cortex_R4_0: -->Sending Erase command to device...
[11/2/2022, 10:21:12 AM] [SUCCESS] Cortex_R4_0: -->Erase storage completed successfully!
[11/2/2022, 10:21:12 AM] [INFO] Cortex_R4_0: Downloading [META_IMAGE1] size [540100]
[11/2/2022, 10:22:17 AM] [INFO] Cortex_R4_0: SUCCESS!! File type META_IMAGE1 downloaded successfully to SFLASH.
[11/2/2022, 10:22:17 AM] [INFO] Cortex_R4_0: Disconnecting from device on COM port COM19...
[11/2/2022, 10:22:17 AM] [INFO] Cortex_R4_0: Flashing instance clean-up initiated...
[11/2/2022, 10:22:17 AM] [INFO] Cortex_R4_0: Instance deinitialized!
[11/2/2022, 10:22:17 AM] [SUCCESS] Program Load completed successfully.
如果是在TI官网上购买的,可以按照以下方式联系客户支持部门的技术部门,会有技术客服为您提供帮助。