This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000-Q1: 参考TIDA-00322 汽车类超声波液位/质量测量参考设计做烟气流速遇到的问题

Part Number: TDC1000-Q1
Other Parts Discussed in Thread: UCC27531

您好:

      我们参考该设计(TIDA-00322 参考设计 | 德州仪器 TI.com.cn)做了一版,用于测试管道烟气流速,目前我们选型的换能器参数如下:

频率 f(kHz):76kHz±4%

带宽△f:±2%

静态电容(pf):1.00nF±20%

阻抗值Z(Ω):300Ω±30%

最大工作电压 脉冲波(占空比2%):<600V

1、如下地方的一些阻容,我们不知道如何正确的设置,还请您帮我们计算一下,谢谢

下图(或文件)中的C22,R36,C32,C23,R37,C30,R39,R26,R30,C20,R34

TIDRBI0.pdf

2、基于78KHz的换能器频率,LNA Gain应该工作在Resistive Feedback Mode是吗?如果是的话LNA的增益还可以做到20dB吗?如何改进?