我们将在春节假期期间对网站进行维护,可能暂时无法访问,同时工程师回复将有所延迟,敬请谅解.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843AOPEVM: Automated Parking Demo in CCS Debug

Part Number: AWR1843AOPEVM
Other Parts Discussed in Thread: AWR1843BOOST

各位前輩們好

我可以在CCS Debug模式下執行.xer4f 與 .xe674

但是當我執行GUI的時候,CCS總會在 exit.c中發生中斷,

[Cortex_R4_0] **********************************************
Debug: Launching the MMW Demo on MSS
**********************************************
Debug: Launched the Initialization Task
Debug: mmWave Control Initialization was successful
Debug: mmWave Control Synchronization was successful
[C674X_0] Debug: DPM Module Sync is done
[Cortex_R4_0] Debug: CLI is operational
Debug: Sending rlRfSetLdoBypassConfig with 3 1 0
Error: DPM Report 4 received with error:-40112 arg0:0x64 arg1:0x8003e88
{module#9}: "../mss_main.c", line 2174: error {id:0x10000, args:[0x1891c, 0x1891c]}
xdc.runtime.Error.raise: terminating execution
[C674X_0] Error: DPM Report 4 received with error:-40112 arg0:0x64 arg1:0x815c9c
xdc.runtime.Main: "../dss_main.c", line 256: assertion failure
xdc.runtime.Error.raise: terminating execution

請問我是否是遺漏了甚麼或還可以檢查什麼呢?

謝謝。

  • 附上Build時候的訊息,不知道與那兩個error是否有關係,

    但是我的環境在lab0014_obstacle_detection_aop是可以正常Debug運作的,

    是否是有哪些環境參數還需要更新呢?謝謝。

    **** Clean-only build of configuration aop for project automated_parking_18xx_mss ****
    
    "C:\\ti\\ccs1200\\ccs\\utils\\bin\\gmake" -k -j 8 clean -O 
     
    DEL /F  "parking_18xx_demo_mss_aop.hex"  "configPkg\linker.cmd" "configPkg\compiler.opt"  "parking_18xx_demo_mss_aop.xer4f" 
    DEL /F "antenna_geometry.oer4f" "mmw_cli.oer4f" "mmw_lvds_stream.oer4f" "mmwdemo_adcconfig.oer4f" "mmwdemo_flash.oer4f" "mmwdemo_monitor.oer4f" "mmwdemo_rfparser.oer4f" "mss_main.oer4f" "objdetrangehwa.oer4f" 
    DEL /F "antenna_geometry.d" "mmw_cli.d" "mmw_lvds_stream.d" "mmwdemo_adcconfig.d" "mmwdemo_flash.d" "mmwdemo_monitor.d" "mmwdemo_rfparser.d" "mss_main.d" "objdetrangehwa.d" 
    RMDIR /S/Q  "configPkg\" 
    找不到 C:\Users\T000090\workspace_v12\automated_parking_18xx_mss\aop\parking_18xx_demo_mss_aop.hex
    Finished clean
     
    
    **** Build Finished ****
    
    **** Build of configuration aop for project automated_parking_18xx_mss ****
    
    "C:\\ti\\ccs1200\\ccs\\utils\\bin\\gmake" -k -j 8 all -O 
     
    Building file: "../mmw_mss.cfg"
    Invoking: XDCtools
    "C:/ti/xdctools_3_50_08_24_core/xs" --xdcpath="C:/ti/bios_6_73_01_01/packages;" xdc.tools.configuro -o configPkg -t ti.targets.arm.elf.R4Ft -p ti.platforms.cortexR:AWR18XX:false:200 -r release -c "C:/ti/ti-cgt-arm_16.9.6.LTS" --compileOptions "--enum_type=int " "../mmw_mss.cfg"
    making package.mak (because of package.bld) ...
    generating interfaces for package configPkg (because package/package.xdc.inc is older than package.xdc) ...
    configuring mmw_mss.xer4ft from package/cfg/mmw_mss_per4ft.cfg ...
    generating custom ti.sysbios library makefile ... 
    Starting build of library sources ...
    making C:/Users/T000090/workspace_v12/automated_parking_18xx_mss/src/sysbios/sysbios.aer4ft ...
    gmake[1]: Entering directory `C:/Users/T000090/workspace_v12/automated_parking_18xx_mss/src/sysbios'
    gmake[1]: Nothing to be done for `all'.
    gmake[1]: Leaving directory `C:/Users/T000090/workspace_v12/automated_parking_18xx_mss/src/sysbios'
    Build of libraries done.
    cler4ft package/cfg/mmw_mss_per4ft.c ...
    Finished building: "../mmw_mss.cfg"
     
    Building file: "../antenna_geometry.c"
    Invoking: Arm Compiler
    "C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/T000090/workspace_v12/automated_parking_18xx_mss" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr18xx/mmw" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/utils" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/objdetrangehwa" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/common" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=OBJDET_NO_RANGE --define=APP_RESOURCE_FILE='<'ti/demo/xwr18xx/mmw/mmw_res.h'>' --define=USE_2D_AOA_DPU --define=XWR18XX_AOP_ANTENNA_PATTERN -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="antenna_geometry.d_raw" --cmd_file="configPkg/compiler.opt"  "../antenna_geometry.c"
    Finished building: "../antenna_geometry.c"
     
    Building file: "../mmwdemo_flash.c"
    Invoking: Arm Compiler
    "C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/T000090/workspace_v12/automated_parking_18xx_mss" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr18xx/mmw" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/utils" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/objdetrangehwa" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/common" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=OBJDET_NO_RANGE --define=APP_RESOURCE_FILE='<'ti/demo/xwr18xx/mmw/mmw_res.h'>' --define=USE_2D_AOA_DPU --define=XWR18XX_AOP_ANTENNA_PATTERN -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="mmwdemo_flash.d_raw" --cmd_file="configPkg/compiler.opt"  "../mmwdemo_flash.c"
    Finished building: "../mmwdemo_flash.c"
     
    Building file: "../mmwdemo_adcconfig.c"
    Invoking: Arm Compiler
    "C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/T000090/workspace_v12/automated_parking_18xx_mss" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr18xx/mmw" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/utils" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/objdetrangehwa" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/common" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=OBJDET_NO_RANGE --define=APP_RESOURCE_FILE='<'ti/demo/xwr18xx/mmw/mmw_res.h'>' --define=USE_2D_AOA_DPU --define=XWR18XX_AOP_ANTENNA_PATTERN -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="mmwdemo_adcconfig.d_raw" --cmd_file="configPkg/compiler.opt"  "../mmwdemo_adcconfig.c"
    Finished building: "../mmwdemo_adcconfig.c"
     
    Building file: "../mmwdemo_monitor.c"
    Invoking: Arm Compiler
    "C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/T000090/workspace_v12/automated_parking_18xx_mss" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr18xx/mmw" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/utils" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/objdetrangehwa" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/common" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=OBJDET_NO_RANGE --define=APP_RESOURCE_FILE='<'ti/demo/xwr18xx/mmw/mmw_res.h'>' --define=USE_2D_AOA_DPU --define=XWR18XX_AOP_ANTENNA_PATTERN -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="mmwdemo_monitor.d_raw" --cmd_file="configPkg/compiler.opt"  "../mmwdemo_monitor.c"
    Finished building: "../mmwdemo_monitor.c"
     
    Building file: "../mmwdemo_rfparser.c"
    Invoking: Arm Compiler
    "C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/T000090/workspace_v12/automated_parking_18xx_mss" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr18xx/mmw" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/utils" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/objdetrangehwa" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/common" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=OBJDET_NO_RANGE --define=APP_RESOURCE_FILE='<'ti/demo/xwr18xx/mmw/mmw_res.h'>' --define=USE_2D_AOA_DPU --define=XWR18XX_AOP_ANTENNA_PATTERN -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="mmwdemo_rfparser.d_raw" --cmd_file="configPkg/compiler.opt"  "../mmwdemo_rfparser.c"
    Finished building: "../mmwdemo_rfparser.c"
     
    Building file: "../objdetrangehwa.c"
    Invoking: Arm Compiler
    "C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/T000090/workspace_v12/automated_parking_18xx_mss" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr18xx/mmw" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/utils" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/objdetrangehwa" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/common" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=OBJDET_NO_RANGE --define=APP_RESOURCE_FILE='<'ti/demo/xwr18xx/mmw/mmw_res.h'>' --define=USE_2D_AOA_DPU --define=XWR18XX_AOP_ANTENNA_PATTERN -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="objdetrangehwa.d_raw" --cmd_file="configPkg/compiler.opt"  "../objdetrangehwa.c"
    Finished building: "../objdetrangehwa.c"
     
    Building file: "../mmw_lvds_stream.c"
    Invoking: Arm Compiler
    "C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/T000090/workspace_v12/automated_parking_18xx_mss" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr18xx/mmw" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/utils" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/objdetrangehwa" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/common" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=OBJDET_NO_RANGE --define=APP_RESOURCE_FILE='<'ti/demo/xwr18xx/mmw/mmw_res.h'>' --define=USE_2D_AOA_DPU --define=XWR18XX_AOP_ANTENNA_PATTERN -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="mmw_lvds_stream.d_raw" --cmd_file="configPkg/compiler.opt"  "../mmw_lvds_stream.c"
    Finished building: "../mmw_lvds_stream.c"
     
    Building file: "../mmw_cli.c"
    Invoking: Arm Compiler
    "C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/T000090/workspace_v12/automated_parking_18xx_mss" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr18xx/mmw" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/utils" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/objdetrangehwa" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/common" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=OBJDET_NO_RANGE --define=APP_RESOURCE_FILE='<'ti/demo/xwr18xx/mmw/mmw_res.h'>' --define=USE_2D_AOA_DPU --define=XWR18XX_AOP_ANTENNA_PATTERN -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="mmw_cli.d_raw" --cmd_file="configPkg/compiler.opt"  "../mmw_cli.c"
    Finished building: "../mmw_cli.c"
     
    Building file: "../mss_main.c"
    Invoking: Arm Compiler
    "C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --include_path="C:/Users/T000090/workspace_v12/automated_parking_18xx_mss" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr18xx/mmw" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/utils" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/objdetrangehwa" --include_path="C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpc/objectdetection/common" --include_path="C:/ti/ti-cgt-arm_16.9.6.LTS/include" --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=OBJDET_NO_RANGE --define=APP_RESOURCE_FILE='<'ti/demo/xwr18xx/mmw/mmw_res.h'>' --define=USE_2D_AOA_DPU --define=XWR18XX_AOP_ANTENNA_PATTERN -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f --preproc_with_compile --preproc_dependency="mss_main.d_raw" --cmd_file="configPkg/compiler.opt"  "../mss_main.c"
    Finished building: "../mss_main.c"
     
    Building target: "parking_18xx_demo_mss_aop.xer4f"
    Invoking: Arm Linker
    "C:/ti/ti-cgt-arm_16.9.6.LTS/bin/armcl" -mv7R4 --code_state=16 --float_support=VFPv3D16 -me -O3 --define=SOC_XWR18XX --define=SUBSYS_MSS --define=DOWNLOAD_FROM_CCS --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --define=DebugP_ASSERT_ENABLED --define=_LITTLE_ENDIAN --define=OBJDET_NO_RANGE --define=APP_RESOURCE_FILE='<'ti/demo/xwr18xx/mmw/mmw_res.h'>' --define=USE_2D_AOA_DPU --define=XWR18XX_AOP_ANTENNA_PATTERN -g --diag_warning=225 --diag_wrap=off --display_error_number --gen_func_subsections=on --enum_type=int --abi=eabi --obj_extension=.oer4f -z -m"parking_18xx_demo_mss_aop.map" --heap_size=0x800 --stack_size=0x800 -i"C:/ti/ti-cgt-arm_16.9.6.LTS/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/control/mmwave/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/control/mmwavelink/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/control/dpm/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/adcbuf/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/crc/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/dma/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/edma/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/esm/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/gpio/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/hwa/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/mailbox/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/osal/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/pinmux/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/soc/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/uart/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/qspi/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/qspiflash/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/utils/cli/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/utils/mathutils/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpu/rangeproc/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/datapath/dpedma/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/drivers/cbuff/lib" -i"C:/ti/mmwave_sdk_03_05_00_04/packages/ti/utils/hsiheader/lib" -i"C:/ti/ti-cgt-arm_16.9.6.LTS/include" --reread_libs --disable_auto_rts --define=MMWAVE_L3RAM_NUM_BANK=6 --define=MMWAVE_SHMEM_TCMA_NUM_BANK=0 --define=MMWAVE_SHMEM_TCMB_NUM_BANK=0 --define=MMWAVE_SHMEM_BANK_SIZE=0x20000 --diag_error=10015 --diag_warning=225 --diag_wrap=off --display_error_number --warn_sections --xml_link_info="xwr18xx_mmw_demo_mss_linkInfo.xml" --rom_model --unused_section_elimination=on -o "parking_18xx_demo_mss_aop.xer4f" "./antenna_geometry.oer4f" "./mmw_cli.oer4f" "./mmw_lvds_stream.oer4f" "./mmwdemo_adcconfig.oer4f" "./mmwdemo_flash.oer4f" "./mmwdemo_monitor.oer4f" "./mmwdemo_rfparser.oer4f" "./mss_main.oer4f" "./objdetrangehwa.oer4f" "../mmw_mss_linker.cmd" "../r4f_linker.cmd" -l"configPkg/linker.cmd"  -llibosal_xwr18xx.aer4f -llibesm_xwr18xx.aer4f -llibgpio_xwr18xx.aer4f -llibsoc_xwr18xx.aer4f -llibpinmux_xwr18xx.aer4f -llibcrc_xwr18xx.aer4f -llibuart_xwr18xx.aer4f -llibqspi_xwr18xx.aer4f -llibqspiflash_xwr18xx.aer4f -llibmailbox_xwr18xx.aer4f -llibmmwavelink_xwr18xx.aer4f -llibmmwave_xwr18xx.aer4f -llibadcbuf_xwr18xx.aer4f -llibdma_xwr18xx.aer4f -llibedma_xwr18xx.aer4f -llibcli_xwr18xx.aer4f -llibhwa_xwr18xx.aer4f -llibdpm_xwr18xx.aer4f -llibmathutils.aer4f -llibcbuff_xwr18xx.aer4f -llibhsiheader_xwr18xx.aer4f -llibrangeproc_hwa_xwr18xx.aer4f -llibdpedma_hwa_xwr18xx.aer4f -lrtsv7R4_T_le_v3D16_eabi.lib -llibc.a 
    <Linking>
    Finished building target: "parking_18xx_demo_mss_aop.xer4f"
     
    rm -f C:/Users/T000090/workspace_v12/automated_parking_18xx_mss/parking_18xx_demo_aop.bin
    makefile:202: recipe for target 'post-build' failed
    process_begin: CreateProcess(NULL, rm -f C:/Users/T000090/workspace_v12/automated_parking_18xx_mss/parking_18xx_demo_aop.bin, ...) failed.
    make (e=2): 系統找不到指定的檔案。
     
    gmake[2]: [post-build] Error 2 (ignored)
    C:/ti/mmwave_sdk_03_05_00_04/packages/scripts/ImageCreator/out2rprc/out2rprc.exe parking_18xx_demo_mss_aop.xer4f parking_18xx_demo_mss_aop.tmp
    Parsing the input object file, parking_18xx_demo_mss_aop.xer4f.
    Appending zeros 0
    Appending zeros 256
    Appending zeros 119416
    File conversion complete!
    C:/ti/mmwave_sdk_03_05_00_04/packages/scripts/ImageCreator/multicore_image_generator/MulticoreImageGen.exe LE 37 0x00000008 parking_18xx_demo_aop.bin 0x35510000 parking_18xx_demo_mss_aop.tmp 0xb5510000 C:/ti/mmwave_sdk_03_05_00_04/firmware/radarss/xwr18xx_radarss_rprc.bin 0xd5510000 C:/Users/T000090/workspace_v12/automated_parking_18xx_dss/aop/parking_18xx_demo_dss_aop.bin
    Number of Input Files 3
    Number of zeros 8
    Number of zeros 48
     
    C:/ti/mmwave_sdk_03_05_00_04/packages/scripts/ImageCreator/crc_multicore_image/crc_multicore_image.exe parking_18xx_demo_aop.bin parking_18xx_demo_aop.tmp
    size of App Image is 323264 bytes
    cur_crc_read_addr 128
    cur_crc_read_addr 124800
    cur_crc_read_addr 159680
    Failed to remove CRC temp file
     
    C:/ti/mmwave_sdk_03_05_00_04/packages/scripts/ImageCreator/append_bin_crc/gen_bincrc32.exe parking_18xx_demo_aop.bin
    >>>> Binary CRC32 = 254d820d <<<<
    >>>> Total bytes in binary file 323268 <<<<
     
     
    
    **** Build Finished ****
    

  • 请问用的是哪个版本的toolbox? 如果直接烧写到flash里,GUI里能正确显示吗?

  • Hi Shine

    感謝回覆

    在使用mmwave_automotive_toolbox_3_6_0xwr18xx_mmw_aop_demo.bin + GUI是OK的。

    但是使用

    mmwave_sdk_03_06_00_00 mmwave_sdk_03_05_00_04xwr18xx_ccsdebug.bin

    mmwave_automotive_toolbox_3_6_0xwr18xx_mmw_aop_demo_dss.xe674xwr18xx_mmw_aop_demo_mss.xer4f會發生以上狀況,

    IDE如下,請問有其他版本建議或是我那些參數可能設錯了呢?

    謝謝。

  • Hi Shine

    感謝協助,

    我有找到解決的方法了,但是不知道為什麼,

    AWR1843AOP: Code stops running after sending sensor start

    請問您有有關這問題的後續嗎?或是原因呢?

    謝謝。

  • 请问如果用prebuilt_binaries里的代码会有这个问题吗?

  • Hi Shine

    是的,如上面所述,prebuilt_binaries 裡面的 .bin 不會有這問題,但是 .xe674 和 .xer4f 是會有一樣問題的。

  • e2e工程师需要验证一下是不是个bug,请看下面工程师的回复。

    Please give us some time to reproduce this issue.

    It is possible that it is a bug

    In the mean time,

    If the customer has also a AWR1843BOOST board, please ask him to try on that board.

  • Hi Shine

    感謝您的協助,AWR1843BOOST是OK,但AOP必須降低numLoops 才會正常

  • 看到您直接回复e2e工程师了,感谢告知!

  • e2e工程师有最新回复。请发一下您板子正面和反面的硬件配置。

    Could you send a picture of your hardware setup, back and front? 

  • 请看e2e工程师的最新回复。
    I was able to run the demo as it is without making any changes to the numLoops which leads me to believe there might be something else causing the error. I also got a similar error where the software would stop after sending sensor start but it was resolved after entering the correct pin configuration. Overall, I would recommend to recheck your setup and go over your execution steps once more. 

  • Hi Shine

    感謝協助,雖然沒得到為什麼會有這現象,但至少知道降低numLoops 是可以正常運作的,

    也只能先ˋ這樣繼續測試了,

    再次感謝您的協助,謝謝。

  • 不客气~

    感谢理解!