Other Parts Discussed in Thread: DCA1000EVM, MMWAVEICBOOST, IWR1642BOOST, UNIFLASH
安装mmwave_studio_user_guide.pdf 要求安装了一系列软件,但是mmwave_studio软件空白。

英文论坛上面的相关回答:
Are you sure you downloaded all the below softwares :
1. 32-bit Matlab Runtime Engine (Version 8.5.1)
2. FTDI Drivers: FTDI USB Driver (mmwave_studio_\mmWaveStudio\ftdi) necessary to work with Radar device is installed.
3. Microsoft Visual C++ 2013 Redistributable package
Maybe the package and all the related software didn't download properly. You could try the installation process once again after uninstalling.
上述步骤都已经完成!但是打开mmwave_studio软件还是空白的。
英文论坛后面还说:
Also make sure the above combination of DCA1000 and XWR BOOST-EVM are connected to the PC while opening mmWaveStudio for the first time.
这里面的意思是如果有DCA1000和XWR BOOST-EVM ,则必须连接PC吧?而不是说AWR6843AOPEVM 必须跟DCA1000和XWR BOOST-EVM连接才能工作吧?AWR6843AOPEVM 本身可以连接电脑并用软件打开使用吧?
如何才能得到下图的软件界面:

我的硬件如图所示:

之前了解到必须要DCA1000EVM Data Capture Card才能采集原始数据,如果想要运行DCA1000EVM ,必须搭配使用MMWAVEICBOOST?
看到用户手册上描述:DCA1000 EVM 必须由 5V 电源以及与 MMWAVEICBOOST 和天线模块连接到同一 PC 的 micro-USB 以太网线缆供电。
但是图 4-15. 提供了采用 xWR6843AOPEVM 和 DCA1000EVM 的设置,好像又可以配套AWR6843AOPEVM 和 DCA1000EVM 使用。请回答。

期待尽快回复!
祝好!
何密