This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843: iwr1843:CANFD无法接收数据

Part Number: IWR1843
Other Parts Discussed in Thread: SYSBIOS

CANFD 设置经典模式,可以成功发送数据给上位机,可以进入发送中断;

但是不能接收上位机下发的数据,进不了接收中断函数。

  • 请问有对例程做修改吗?CAN管脚上能测量到上位机发的时序吗?如果时序正确,接收中断标志位是否有置起来?

  • 例程基本没做修改;CAN能发送数据,时序应该是是对的;

    但是上位机发送数据时会出现崩溃;

    [Cortex_R4_0] Exception occurred in ThreadType_Main.
    Main handle: 0x0.
    Main stack base: 0x8013488.
    Main stack size: 0x1000.
    R0 = 0x0000ac90 R8 = 0x00080000
    R1 = 0x00002890 R9 = 0x00000000
    R2 = 0x08014b38 R10 = 0x00000000
    R3 = 0x08013488 R11 = 0xff500000
    R4 = 0x00000000 R12 = 0x08014a74
    R5 = 0x0000ac90 SP(R13) = 0x00000000
    R6 = 0x0000f044 LR(R14) = 0x00008f14
    R7 = 0x0000f088 PC(R15) = 0x00002890
    PSR = 0x600c019f
    DFSR = 0x00000808 IFSR = 0x00000000
    DFAR = 0xfffffff8 IFAR = 0x00000000
    ti.sysbios.family.arm.exc.Exception: line 205: E_dataAbort: pc = 0x00002890, lr = 0x00008f14.
    xdc.runtime.Error.raise: terminating execution

  • 接收函数赋值给回调函数,接收标志位接收完 gRxDoneFlag = 1;

    mcanCfgParams->appDataCallBack      = MCANAppCallback;

    static void MCANAppCallback(CANFD_MsgObjHandle handle, CANFD_Reason reason)
    {
    Task_Params UART_taskParams;

    int32_t errCode, retVal;
    uint32_t id;
    CANFD_MCANFrameType rxFrameType;
    CANFD_MCANXidType rxIdType;
    if (reason == CANFD_Reason_TX_COMPLETION)
    { {
    gTxPkts++;
    gTxDoneFlag = 1;
    return;
    } }
    if (reason == CANFD_Reason_RX)
    { {
    /* Reset the receive buffer */
    memset(&rxData, 0, sizeof (rxData));
    dataLength = 0;
    retVal = CANFD_getData (handle, &id, &rxFrameType, &rxIdType, &rxDataLength,&rxData[0], &errCode);
    //if (retVal < 0)
    //{
    // System_printf ("Error: CAN receive data for iteration %d failed [Error code %d]\n", iterationCount, errCode);
    // return;
    //}

    /* Validate the data */
    gRxPkts++;
    gRxDoneFlag = 1;
    return;
    } }
    if (reason == CANFD_Reason_TX_CANCELED)
    { {
    gTxPkts++;
    gTxDoneFlag = 1;
    gRxDoneFlag = 1;
    return;
    } }
    }