This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: 噪声系数波动过大,在有些频点符合预期,在某些频点很差

Part Number: AWR2243BOOST
Other Parts Discussed in Thread: AWR2243

我们使用AWR2243 BOOST进行测试,通过mmWave-Radar-Interface-Control文档中提到的监控项AWR_MONITOR_RX_NOISE_FIGURE_REPORT_AE_SB读取各芯片在77GHz/78GHz/79GHz/80GHz/81GHz附近的噪声系数。

波形配置完全相同情况下,噪声系数差别较大。在79GHz下,噪声系数在15dB到20dB之间波动,而在80GHz下,噪声系数基本在14dB左右。并且不同芯片也有一定差异,芯片4(从芯片3)最稳定,芯片1(主芯片)波动最大。 我们期望的噪声系数稳定在12dB或者15dB,但是目前在有些频点波动10dB左右,导致检测不稳定,该如何解决。

波形参数如下:

profileId=0;
pfVcoSelect=2;
startFreqConst=1472666737;//79G
idleTimeConst=200;//2000ns
adcStartTimeConst=279;//2790ns
rampEndTime=6000;//60000ns
txOutPowerBackoffCode=0;//发射功率衰减0db
txPhaseShifter=0;//移相器配置0度
freqSlopeConst=28;//1351.812kHZ/us
txStartTime=0;//0ns
numAdcSamples=512;//512
digOutSampleRate=9230;//9230ksps
hpfCornerFreq1=0;
hpfCornerFreq2=0;
rxGain=48;//48db

在实际使用中也发现,80GHz探测距离确实比79GHz更远。