This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243BOOST: tx2的信号强度比tx0和tx1低约10倍,但不知道在哪设置调整到一样

Part Number: AWR2243BOOST

我尝试在AWR2243BOOST上把TX0,TX1,TX2都用上。    我的设置流程如下:

1. 先运行scripts文件夹下的DataCaptureDemo_xWR.lua文件将基础的设置走通, 确认可以用TX0采集1发4收的信号。

2. 按照下图在staticconfig界面中打开TX1和TX2

3. 按照下图在sensorconfig中的chirp界面设置好3个TX,  按TDM的MIMO方法。

4. 按照下图在sensorconfig中的frame界面设置好相关参数

5. 分别点击 DCA1000ARM, Trigger Frame, PostProc采集并看结果。  结果如下所示

可以看到TX2的原始信号强度明显低非常多。  

我初步怀疑是在某个位置需要给tx调整信号强度,但是找了一圈都没有找到。