This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1101: LDC1101

Part Number: LDC1101


你好!!!

    我之前使用过 LDC1101EVM 评估板,上面LDC1101的 VDD 是 1.8V,CLKIN 由 MSP430 引脚提供。

    现在我需要绘制自己的 LDC1101 PCB,如果将 VDD 修改为 3.3V,会导致测量结果出现上面变化呢?或者说 会影响 LDC1101 的测量性能吗?同时使用ESP32s3(MCU)的引脚为 LDC1101 提供时钟输入,应该也是可以的吧!!!