Part Number: LDC1101
你好!!!
我之前使用过 LDC1101EVM 评估板,上面LDC1101的 VDD 是 1.8V,CLKIN 由 MSP430 引脚提供。
现在我需要绘制自己的 LDC1101 PCB,如果将 VDD 修改为 3.3V,会导致测量结果出现上面变化呢?或者说 会影响 LDC1101 的测量性能吗?同时使用ESP32s3(MCU)的引脚为 LDC1101 提供时钟输入,应该也是可以的吧!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
只要您保持在建议的电源范围内,LDC1101的性能不会因电源变化而出现太多性能变化。英文论坛也有类似问题咨询,您也可以看下美国工程师的回复:
LDC1101EVM: How does powering the LDC1101 from a voltage other than 1.8V affect performance?
同时使用ESP32s3(MCU)的引脚为 LDC1101 提供时钟输入,应该也是可以的吧!!!
可以,注意电平范围: