This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: 向iwr1443发送 sensorstart 指令时 开发板出现错误

Part Number: IWR1443

尊敬的各位工程师朋友们!

       我调试IWR1443板时遇到了一个棘手的问题:
      首先,我将iwr1443连接到TI的mmWave Demo Visualizer时,会出现cfg文件发送停在sensorStart,

并且出现debug:Debug: Init Calibration Status = 0x3fe

Exception: ../main.c, line 1714.

如下图所示:

这样的错误就会导致:电脑向 iwr1443 发送一次cfg配置文件(因为开发板并未真正执行sensorStart),无法再次发送cfg配置文件到开发板。  iwr1443开发板无法正常工作。    我在使用实验使用iwr1443,就出现启动一次,后续出现无法发送cfg配置文件的错误。
                                                                                                                 真诚的希望各位朋友们能够提出解决方法!