Other Parts Discussed in Thread: IWR6843
我按照教程连接了DCA1000和IWR6843,如下图所示。
然后发现网口一直是黄灯常亮,绿灯闪烁然后不亮:
通过mmwave studio连接时,也是出现了问题,connection是正常的:
而SetUp DCA1000的时候出现了问题:
请问这种问题应该如何解决呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我按照教程连接了DCA1000和IWR6843,如下图所示。
然后发现网口一直是黄灯常亮,绿灯闪烁然后不亮:
通过mmwave studio连接时,也是出现了问题,connection是正常的:
而SetUp DCA1000的时候出现了问题:
请问这种问题应该如何解决呢?
ar1.GetCaptureCardDllVersion()
[11:38:06] [RadarAPI]: Sending dll_version command to DCA1000
[11:38:06] [RadarAPI]:
[11:38:06] DLL Version : 1.0
[11:38:06] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
[11:38:06] [RadarAPI]: Status: Passed
[11:38:12] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
[11:38:12] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30)
[11:38:12] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
没有任何的error报错,点击“connect,reset,and”就一直卡在这个地方不动
请问板子供电电压是5v/3A吗?请按照下面网站上的步骤操作一下。
DCA1000EVM使用指南 - 嵌入式处理 - 技术文章 - E2E 设计支持 (ti.com)