This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: DCA1000

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: DCA1000EVM

我按照指导书配置完成后,在进行Caputer and Post Processing这一步骤出现了错误。

[20:16:13] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
[20:16:13] [RadarAPI]: Sending start_record command to DCA1000
[20:16:20] [RadarAPI]: ar1.StartFrame()
[20:16:20] [RadarAPI]: Status: Passed
[20:16:20] Frame start async event received!
[20:16:20] [RadarAPI]: Frame Ended
[20:17:33] [RadarAPI]:
[20:17:33] Frame End async event received!
[20:17:33] [RadarAPI]:
[20:17:33] Start Record command : Success
[20:17:33]
[20:17:33] LVDS buffer full
[20:17:33]
[20:17:33] Record Process :
[20:17:33] Timeout Error! System disconnected
[20:17:33]
[20:17:33] Record stop is done successfully
[20:17:42] [RadarAPI]: ar1.StartMatlabPostProc("C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\PostProc\\adc_data.bin")
[20:17:42] [RadarAPI]: No of files Captured: 0, Total no of frames for each device : 8
[20:17:42] Error : The number of files captured is zero!