This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV411EVM: ICOMP1、ICOMP2测量0A时输出为4.7V、0.4V

Part Number: DRV411EVM


尊敬的支持团队

                          开发板上安装了AKM的霍尔传感器,型号为:HG-302S,GSEL1拉高(5V)、GSEL2拉低(0V),在上电后不进行测量电流动作,ICOMP1输出4.7V、ICOMP2输出0.4V与规格书描述输出2.5V不符,烦请帮忙看一下是啥问题,原理图如下