之前一直很好的板子,今天拉出来,通电以后, FPGA_RST灯亮红色, 网口连不上, 请帮忙看看原因。

另外看别的帖子说可以用Lattice的Diamond Programmer重新下载FPGA firmware。 但是 Diamond Programmer好像不能直接下载到。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
之前一直很好的板子,今天拉出来,通电以后, FPGA_RST灯亮红色, 网口连不上, 请帮忙看看原因。

另外看别的帖子说可以用Lattice的Diamond Programmer重新下载FPGA firmware。 但是 Diamond Programmer好像不能直接下载到。
使用Diamond Programmer重新烧入FPGA bit,问题依然无法解决。 请问能提供返修服务吗?
您好,
根据您的描述,FPGA_RST灯亮红色且无法连接到网络,可能是由于以下原因之一:
1. 供电问题:首先,请确保评估板的电源供应正常。检查电源线是否插紧,确认电源适配器输出的电压和电流符合评估板的要求。
2. FPGA固件问题:红色的FPGA_RST灯亮起可能意味着FPGA固件加载失败。您可以尝试重新下载FPGA固件来解决问题。确保您使用的是正确的FPGA固件文件,并使用适当的工具进行下载。
3. 硬件故障:如果以上两个方面都没有问题,那么可能是评估板本身出现了硬件故障。在这种情况下,建议您联系德州仪器的技术支持团队,向他们咨询并寻求进一步的帮助。
关于Diamond Programmer不能直接下载的问题,您可以尝试以下方法:
1. 确认连接:首先,请确保您的评估板与电脑通过适当的接口(如USB)连接,并且连接稳定。
2. 安装驱动:确保您已经正确安装了Lattice Diamond软件,并且安装了相应的驱动程序。
3. 选择正确的设备:在Diamond Programmer中,选择正确的设备型号和连接方式,以便与评估板进行通信。
4. 导入FPGA固件:将您要下载的FPGA固件文件导入到Diamond Programmer中,并按照指导进行下载操作。
请按照以下方式联系客户支持部门的技术部门,会有技术客服为您提供帮助。
打开链接https://ticsc.service-now.com/csm
点击申请新的支持下面的提交申请按钮
在新打开的窗口中点击技术帮助下面的创建案例按钮
在打开的表格中您可以使用中文描述您的问题并且递交。递交申请时,请您提及以下信息:
Ti.com购买订单号
需要技术鉴定EVM是否存在质量问题
您是否使用免费邮箱注册myti账号
电源适配器5V,3A。 同一个电源适配器在另外一个DCA1000 试了,没有问题。
这个板子比较贵, 坏了确实挺让人心疼的。
FPGA固件为C:/ti/mmwave_studio_03_00_00_14/mmWaveStudio/PlatformBinaries/DCA1000FPGA/DCA1000_FPGA_RECORD_V2.8_05JUL2019.bit版本,下载过程没有问题。



您好,以下是工程师的回复:
Thanks for the post. You may want to double check your switch positions against the user manual, in case you have moved them. (see Figure 16 specifically, which is different than what you have selected) The re-programming procedure is in this manual, too. https://www.ti.com/lit/ug/spruij4a/spruij4a.pdf
If you are still having issues and have reconnected the Ethernet cable, reconnected the RADAR EVM to the DCA, and double checked that your static IP is set up on your PC, etc. Please do provide some sharper images of your setup as well as any screen shots you can take of where the failure is occurring.
您好,以下是工程师的回复:
thanks for the document. Only difference i can see here is the choice on the SPI flash device.
in the manual it says to choose this on (in the dropdown): SPI-N25Q128A (page 25)
Can you try that out and double check your switch settings, as well, if you are changing them.
Hi Gary,
I use Diamond Programmer 3.11

there is no “SPI-N25Q128A” in the device list. I think "N25Q128A" is equivelent to “SPI-N25Q128A”~

您好,以下是工程师的回复:
In looking at the schematic, if the FPGA is being held in reset only FPGA and the switch SW7 are connected to control the red LED you have on - something physical may have happened to the FPGA on your board. Are you using in ESD safe or protected environment?
您好,抱歉,您只能找购买渠道mouser解决返修问题。TI是没有返修的,如果是在ti.com购买,那就是找CSC解决。其他任何地方买的,只能是哪里买的找哪里
您好,不客气,我将关闭此贴,有问题请随时重新发帖,谢谢!