This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: 1843和dca1000采集的数据大小和bin数据格式类型

Part Number: AWR1843BOOST
Other Parts Discussed in Thread: AWR1642, AWR1843

描述:经查AWR1843的raw data格式可以参考AWR1642的格式,都是2个LVDS lane。只能传输两路通道,我现在使用dca1000 设置的是4RX 3TX 那么就应该可以同时可以处理十二路独立的信号路径

问题1:这里的2lvds lane 和 12路镀锡信号路径 有啥区别

问题2:此时输出的bin文件大小是如何计算的

问题3:此时输出的bin文件是否包含这个12路的独立信号路径

问题4:如何对bin文件进行matble 的12路的 每一路进行1d 2d 等操作

  • 问题1:2个LVDS lane是指AWR1843传输数据的物理通道数量,而12路独立信号路径是指从AWR1843收到的原始数据中可以提取出的独立信号通道数量。这两者的区别在于,2个LVDS lane是AWR1843传输数据的物理通道数量,而12路独立信号路径是可以从这些物理通道中提取出的独立信号通道数量。

    问题2:输出的bin文件大小取决于多个因素,包括采样率、采样深度、数据压缩方式等。在使用dca1000进行数据采集时,可以通过设置采样率、采样深度等参数来控制输出的bin文件大小。一般情况下,输出的bin文件大小与采集时间和数据压缩方式有关。

    问题3:输出的bin文件包含从AWR1843接收到的所有原始数据,包括12路独立信号路径和其他相关数据。可以通过解析bin文件来提取出所需的数据通道。

    问题4:要对bin文件进行matlab的1D、2D等操作,需要先将bin文件导入到matlab中。可以使用matlab的文件读取函数将bin文件读取到matlab中,然后对数据进行处理。在处理数据之前,需要先了解bin文件中数据的格式和存储方式,以便正确读取和解析数据。根据AWR1843的数据格式,可以使用matlab的相关函数进行数据解析和处理。例如,可以使用matlab的reshape函数将一维数据转换为二维数据,以进行2D操作。