如图所示,Visualizer是4,4的版本,电源使用的是12V-3A的
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在这种情况下,出现"Connecting"的情况可能有几种可能的原因。以下是一些可能的解决方法:
1. 确保连接正确:首先确保AWR2944EVM与PC连接正确。检查USB连接线是否插入正确,确保设备管理器中可以看到AWR2944EVM的正确设备。如果有其他连接方式(例如以太网连接),也需要确保连接正确。
2. 检查固件版本:确保mmWave_Demo_Visualizer的固件版本与AWR2944EVM的固件版本兼容。有时候固件版本不匹配会导致连接问题。
3. 检查电源:您提到使用了12V-3A的电源,这个电源应该足够满足AWR2944EVM的需求。但是仍然需要确保电源是稳定的,没有电压波动或者噪声。
4. 检查Visualizer设置:在Visualizer中,确保选择了正确的端口和波特率。有时候选择错误的端口或者波特率也会导致连接问题。
5. 重启设备和软件:有时候重启AWR2944EVM和Visualizer软件也可以解决连接问题。