This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2112: 是否可以将金属管连接至芯片上的引脚,金属管放入液体中来检测液位的变化

Part Number: FDC2112


你好,

是否可以将两跟直径3.1mm的金属管分别连接至芯片FDC2112的IN0A,IN0B引脚上(或IN1A,IN1B引脚),然后将金属管放入液体中;

实际使用中,将金属管放入(洗洁精兑水而成),芯片返回值DATAx会出现反复跳动;

请问是否可以通过这种办法进行液位的检测,而不是感应的方式。