This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944EVM: What are the four UARTs on the AWR2944EVM used for?

Part Number: AWR2944EVM

hi

I am studying the usage of the 2944.

In the manual of the 2944, I learned that the four UARTs have different roles, as shown in the figure.

Question 1: Are the four UARTs referring to MSS UART, DSS UART, BSS UART, and RS232UART?

Question 2: I compared the EVM schematic and the MSS UART connected to XDS110 should be responsible for debugging registers mentioned in the screenshot, am I correct?

Question 3: What functions do the other three UARTs serve? Why is the DSS UART in a disconnected state on the EVM?

Simon

  • four UARTs

    1. Auxiliary boot loader source UART: used as the source of the Bootloader.
    2. Register debugging interface UART (with XDS110 emulator) : used for register debugging.
    3. Universal UART communication support (UART 1/2) : Communicate with UART

    am I correct?

    I think that's right

  • HI Gary

    What you mean is that MSS UART is connected to XDS110, so it should be used as a register debug interface. Then, among RS232 UART, DSS UART, and BSS UART, which one is responsible for bootloading and which one is responsible for UART communication support?

  • Hello Simon,

    I think 232 is used for boot loading, and D/BSS is used for communication support

    Regards,

    Gary

x 出现错误。请重试或与管理员联系。